2022-09-29 5:54 PM
Hello
My borad can bring up from SD card. But can not boot from eMMC. When boot from eMMC. I can't get any message from the console. How can I find the trouble?
Thanks
2022-09-29 11:51 PM
Hi @WHe.1 ,
Can you share exact reference of STM32MP15 sample and eMMC please ?
I understand you succeed to flash the eMMC with CubeProg right ?
Please share the log from SD Card boot .. it might provide us some insight about your platfom configuration setup.
Olivier
2022-10-04 1:41 AM
Hi @WHe.1
In case of low level boot failure, please share Bootrom log. Please have a look to https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_code_overview#Debug_and_Error_messages
and
https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_trace_analyzer
If you don't use default eMMC pins, please share OTP3 and OTP5-7 values you setup.
Note that some eMMC won't boot with silicon Rev.B. See ES0438 for details.
Regards.
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.