2022-05-10 12:46 AM
Hi everyone,
I'm new to using STM32MP1, in particular I bought a STM32MP157A-DK1 and I wanted to know if it was feasible to load Linux with the classic GUI, open a TCP-IP server and run some python code that I had already developed.
Thank you all
Solved! Go to Solution.
2022-05-10 12:57 AM
Hi @Community membereriani ,
Well, that depends what you intend by "Linux with the classic GUI".
STM32MP157A-DK1 is the version of board without embedeed DSI display.
You can have GUI using HDMI output.
STM32MP157A-DK1 is able to load and run OpenSTLinux, specific linux version wich use Weston/Wayland as GUI manager.
For sure you can open TCP-IP server and run some python code.
As you are new with STM32MP1 I recommand you to start with :
And discover what the "Starter Package" already bring for you.
Hope it help
Olivier
2022-05-10 12:57 AM
Hi @Community membereriani ,
Well, that depends what you intend by "Linux with the classic GUI".
STM32MP157A-DK1 is the version of board without embedeed DSI display.
You can have GUI using HDMI output.
STM32MP157A-DK1 is able to load and run OpenSTLinux, specific linux version wich use Weston/Wayland as GUI manager.
For sure you can open TCP-IP server and run some python code.
As you are new with STM32MP1 I recommand you to start with :
And discover what the "Starter Package" already bring for you.
Hope it help
Olivier
2022-05-10 1:07 AM
Hi @Community member
Thanks for the prompt reply
By "Linux with the classic GUI" I mean whether it was possible to load like GNOME or other desktop environments.
thanks for the link, today I'll give it a look.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.