2021-08-11 12:45 AM
sdk: 3.0.0 ver
kernel: 5.10.10
Ethernet cannot be connected in the kernel of version 5.10.10, but version 5.4.31 works normally
The Ethernet related device tree is as follows:
dts as follows;
ðernet0 {
status = "okay";
pinctrl-0 = <ðernet0_rgmii_pins_a>;
pinctrl-1 = <ðernet0_rgmii_sleep_pins_a>;
pinctrl-names = "default", "sleep";
phy-mode = "rgmii";
max-speed = <1000>;
phy-handle = <&phy0>;
nvmem-cells = <ðernet_mac_address>;
nvmem-cell-names = "mac-address";
mdio0 {
// reset-gpios = <&gpiog 0 GPIO_ACTIVE_LOW>;
// reset-duration = <200>;
#address-cells = <1>;
#size-cells = <0>;
compatible = "snps,dwmac-mdio";
phy0: ethernet-phy@6 {
reg = <6>;
};
};
};
dmesg log as follows:
[ 4.133408] systemd[1]: System time before build time, advancing clock.
[ 6.200429] NET: Registered protocol family 10
[ 6.253839] Segment Routing with IPv6
[ 6.291489] systemd[1]: systemd 247 running in system mode. (-PAM -AUDIT -SELINUX -IMA -APPARMOR -SMACK -SYSVINIT -UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS -ACL -XZ -LZ4 -ZSTD -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[ 6.313175] systemd[1]: Detected architecture arm.
[ 6.383833] systemd[1]: Set hostname to <mc-printer>.
[ 7.212762] systemd[1]: Queued start job for default target Multi-User System.
[ 7.273292] systemd[1]: Created slice system-modprobe.slice.
[ 7.315180] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ 7.352904] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ 7.392807] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ 7.433008] systemd[1]: Reached target Paths.
[ 7.462428] systemd[1]: Reached target Remote File Systems.
[ 7.502287] systemd[1]: Reached target Slices.
[ 7.532420] systemd[1]: Reached target Swap.
[ 7.573156] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
[ 7.581202] systemd[1]: Listening on Journal Socket (/dev/log).
[ 7.623519] systemd[1]: Listening on Journal Socket.
[ 7.663889] systemd[1]: Listening on Network Service Netlink Socket.
[ 7.703797] systemd[1]: Listening on udev Control Socket.
[ 7.743323] systemd[1]: Listening on udev Kernel Socket.
[ 7.783604] systemd[1]: Condition check resulted in Huge Pages File System being skipped.
[ 7.797464] systemd[1]: Mounting POSIX Message Queue File System...
[ 7.839723] systemd[1]: Mounting Kernel Debug File System...
[ 7.879416] systemd[1]: Mounting Kernel Trace File System...
[ 7.920730] systemd[1]: Mounting Temporary Directory (/tmp)...
[ 7.960174] systemd[1]: Starting Create list of static device nodes for the current kernel...
[ 8.019389] systemd[1]: Starting Load Kernel Module configfs...
[ 8.059383] systemd[1]: Starting Load Kernel Module fuse...
[ 8.092664] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[ 8.113030] systemd[1]: Starting Journal Service...
[ 8.147432] systemd[1]: Condition check resulted in Load Kernel Modules being skipped.
[ 8.161475] systemd[1]: Starting Remount Root and Kernel File Systems...
[ 8.214636] systemd[1]: Starting Apply Kernel Variables...
[ 8.220899] EXT4-fs (mmcblk1p6): re-mounted. Opts: (null)
[ 8.259090] systemd[1]: Starting Coldplug All udev Devices...
[ 8.328695] systemd[1]: Mounted POSIX Message Queue File System.
[ 8.364426] systemd[1]: Mounted Kernel Debug File System.
[ 8.403315] systemd[1]: Started Journal Service.
[ 8.857774] systemd-journald[111]: Received client request to flush runtime journal.
[ 8.899170] systemd-journald[111]: File /var/log/journal/7ed74cbb68864e24a4224adbaf2dac03/system.journal corrupted or uncleanly shut down, renaming and replacing.
[ 10.201362] systemd-journald[111]: File /var/log/journal/7ed74cbb68864e24a4224adbaf2dac03/user-1003.journal corrupted or uncleanly shut down, renaming and replacing.
[ 11.092287] systemd-journald[111]: File /var/log/journal/7ed74cbb68864e24a4224adbaf2dac03/user-1004.journal corrupted or uncleanly shut down, renaming and replacing.
[ 11.385051] stm32-hash 54002000.hash: will run requests pump with realtime priority
[ 11.482768] stm32-hash 54002000.hash: Init HASH done HW ver 23 DMA mode 1
[ 11.816408] stm32-crc32 58009000.crc: Initialized
[ 14.023643] 8021q: 802.1Q VLAN Support v1.8
[ 14.252262] etnaviv etnaviv: bound 59000000.gpu (ops gpu_ops [etnaviv])
[ 14.257465] etnaviv-gpu 59000000.gpu: model: GC400, revision: 4652
[ 14.302651] etnaviv-gpu 59000000.gpu: Need to move linear window on MC1.0, disabling TS
[ 14.332750] [drm] Initialized etnaviv 1.3.0 20151214 for etnaviv on minor 0
[ 14.968889] Bluetooth: Core ver 2.22
[ 14.971183] NET: Registered protocol family 31
[ 15.034953] Bluetooth: HCI device and connection manager initialized
[ 15.039905] Bluetooth: HCI socket layer initialized
[ 15.102095] Bluetooth: L2CAP socket layer initialized
[ 15.105785] Bluetooth: SCO socket layer initialized
[ 15.797632] Bluetooth: HCI UART driver ver 2.3
[ 15.800648] Bluetooth: HCI UART protocol H4 registered
[ 15.865822] Bluetooth: HCI UART protocol Broadcom registered
[ 16.003634] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 16.015360] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 16.303090] Bluetooth: hci0: BCM: chip id 121
[ 16.306479] Bluetooth: hci0: BCM: features 0x0e
[ 16.311817] Bluetooth: hci0: BCM4359C0
[ 16.314382] Bluetooth: hci0: BCM4359C0 (003.001.006) build 0000
[ 16.360988] Bluetooth: hci0: BCM4359C0 'brcm/BCM4359C0.hcd' Patch
[ 17.094771] Bluetooth: hci0: BCM43596 UART 37.4MHz AMPAK AP6359S2 CL2[Version: Version: 0149.0331]
[ 17.102426] Bluetooth: hci0: BCM4359C0 (003.001.006) build 0331
[ 17.221839] systemd-journald[111]: File /var/log/journal/7ed74cbb68864e24a4224adbaf2dac03/user-1000.journal corrupted or uncleanly shut down, renaming and replacing.
[ 17.440139] systemd-journald[111]: File /var/log/journal/7ed74cbb68864e24a4224adbaf2dac03/user-1001.journal corrupted or uncleanly shut down, renaming and replacing.
[ 17.508557] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:06] driver [Qualcomm Atheros AR8035] (irq=POLL)
[ 17.542005] dwmac4: Master AXI performs any burst length
[ 17.545958] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found
[ 17.582045] stm32-dwmac 5800a000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported
[ 17.626003] stm32-dwmac 5800a000.ethernet eth0: registered PTP clock
[ 17.638891] stm32-dwmac 5800a000.ethernet eth0: configuring for phy/rgmii link mode
[ 17.662361] brcmfmac: brcmf_fw_alloc_request: using brcm/brcmfmac4359-sdio for chip BCM4359/9
[ 17.673022] cryptd: max_cpu_qlen set to 1000
[ 17.689479] 8021q: adding VLAN 0 to HW filter on device eth0
[ 17.707697] stm32-dwmac 5800a000.ethernet eth0: Adding VLAN ID 0 is not supported
[ 17.952630] brcmfmac: brcmf_fw_alloc_request: using brcm/brcmfmac4359-sdio for chip BCM4359/9
[ 17.959914] brcmfmac: brcmf_c_process_clm_blob: no clm_blob available (err=-2), device may have limited channels available
[ 17.992666] brcmfmac: brcmf_c_preinit_dcmds: Firmware: BCM4359/9 wl0: Apr 22 2019 15:46:28 version 9.87.51.11.31 (1140361@shgit) (r) FWID 01-e64dfcc7
[ 18.962244] ieee80211 phy0: brcmf_dongle_roam: WLC_SET_ROAM_TRIGGER error (-52)
[ 20.793998] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 20.801055] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 22.891077] systemd-journald[111]: File /var/log/journal/7ed74cbb68864e24a4224adbaf2dac03/user-1005.journal corrupted or uncleanly shut down, renaming and replacing.
2021-08-26 5:55 AM
Hi,
did you progress meanwhile ?
from the log above, seems ethernet if OK.
Did you cross check the DTS potential changes between ecosystem V3 (kernel 5.10) and V2 (kernel 5.4) ?
I know that there was some changes regarding driving reset signal. Did you use it on your board ?
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.