2022-08-11 4:23 AM
Hi,
We are using stm32mp157a-dk1 board.So we want to change the default console serial port(UART4) to anthour serial port(UART 7). I have changed respective .dts files in uboot it is working properly up to uboot.Know i want to change in kernal.
So i Refereed St wiki.They said that we need to enable to CONFIG_DEBUG_LL, CONFIG_STM32MP1_DEBUG_UART and CONFIG_EARLY_PRINTK using the Linux Menuconfig.
Refer below link for your reference
https://wiki.st.com/stm32mpu/wiki/Dmesg_and_Linux_kernel_log#earlyprintk
I am unable to active those configurations through linux menuconfig. I am using linux-5.13 version. How can i activate CONFIG_DEBUG_LL, CONFIG_STM32MP1_DEBUG_UART and CONFIG_EARLY_PRINTK?
I am attaching my screenshots for linux-menuconfig and my uboot log.
could you please help us in this regards.
2022-08-31 9:34 AM
Hi @Sindhu Vadde
Don't know it this is the root cause, but Kernel 5.13 is not supported by OpenSTLinux ecosystem, it is either 5.10 with Ecosystem 3.x or 5.15 with Ecosystem 4.x .
Regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.