2026-02-27 8:53 AM - edited 2026-03-18 5:39 AM
Hi,
I’m working with a MYIR MYD-YA157C (STM32MP157AAC) board and I’m trying to restore a board using STM32CubeProgrammer (USB / DFU mode) with a FlashLayout TSV.
The board is custom made , but the HW should not be a problem
But i am running into erorr:
16:47:55 : Download in Progress:
16:47:56 : Error: failed to download Sector[0]
16:47:56 : Error: failed to download the File
16:47:56 : Error: Download partition 0x21 failed
16:47:56 : Error: TSV flashing service failed
16:47:56 : Disconnected from device.
Little bit of a background
The chip comes with preloaded yocto , and after trying to flash our distro we get this erorr
I tried the following things
Remove everything from the EMMC - Nothing helps
Chaning offsets - Did not help
Use UDF tool - Did not help
Tried on different computer - Did not help
Tried different cable - Did not help
It is very strange
I attached logs from Cube programmer
Could somebody help us with some suggestions
2026-03-26 3:47 AM
Hi @lepot
I advise you to contact Myrtech support at fist
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.