2022-12-10 7:04 AM
Dear experts.
we plan to use a STM32MP157, where the A7 core should have 512MB DDR RAM, and theM4 core 16 MB. What options exists, to give the M4 core that 16 MB of RAM?
Is there an application note, showing how more then a MB RAM is added to the M4 core in an STM32MP15x?
Best regards,
Michael
Solved! Go to Solution.
2022-12-12 1:32 AM
Hi @Michael Schmid
please have a look to https://wiki.st.com/stm32mpu/wiki/Exchanging_buffers_with_the_coprocessor
Note that this stand only for Data. Code should reside in SRAMs/RETRAM as Cortex-M4 performance execution penalty for running code from external memory will be extremely high (has there is no caches and bus paths are not optimized for that).
Regards.
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2022-12-10 9:27 AM
> From the DS, i understand that the DDR RAM of the A7 is not accessible for the M4. Is that right?
No, you can assign some DDR RAM space for M4 code and data. This is actually the standard way, the M4 is considered a Linux coprocessor that is booted from Linux (or the bootloader). See https://wiki.st.com/stm32mpu/wiki/Arm_Cortex-M4 and or the STM32MP157 DK2 board schematics
hth
KnarfB
2022-12-12 1:32 AM
Hi @Michael Schmid
please have a look to https://wiki.st.com/stm32mpu/wiki/Exchanging_buffers_with_the_coprocessor
Note that this stand only for Data. Code should reside in SRAMs/RETRAM as Cortex-M4 performance execution penalty for running code from external memory will be extremely high (has there is no caches and bus paths are not optimized for that).
Regards.
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2023-10-10 5:50 AM
Hi,
just one comment about QSPI / SPI, even it might be limited BW.
QSPI Memory controller is designed for NOR as you mentionned. QSPI PSRAM could be used, but controller doesn't support Memory mapped write. APS1604M..., APS6404L..., APS12804O... IoT RAM are example of SPI & QSPI PSRAM (in SOP8/USON8/WLCSP).
Alex
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.