2022-09-12 10:11 AM
Hi.
Some examples use ltdc_ep0_out / reg 0, while others use ltdc_ep1_out / reg 1.
e.g.
https://community.st.com/s/question/0D50X0000BG0RAWSQ3/stm32mp1-ltdc-device-tree-for-rgb-display
Where can I find more details on when to use reg 0 vs reg 1?
<dc {
port {
ltdc_ep1_out: endpoint@1 {
reg = <1>;
remote-endpoint = <&panel_rgb_in>;
};
};
};Thank you
-- Peter
2022-09-13 7:58 AM
Hello @petero ,
Referring to the documentation (Documentation/devicetree/bindings/display/st,stm32-ltdc.yaml), you can find this information:
********************************************************
port:
$ref: /schemas/graph.yaml#/properties/port
description: |
Video port for DPI RGB output.
ltdc has one video port with up to 2 endpoints:
- for external dpi rgb panel or bridge, using gpios
- for internal dpi input of the MIPI DSI host controller
Note: These 2 endpoints cannot be activated simultaneously.
********************************************************
It seems that the number linked with the endpoint has no impact on the DT, that is not the case with DSI for example.
Erwan.
2022-09-13 8:19 AM
@petero ,
As a comparison, if the number of the port/endpoint has an impact, you will see the following thing in the yaml (example of Documentation/devicetree/bindings/display/st,stm32-dsi.yaml):
***************************************
ports:
$ref: /schemas/graph.yaml#/properties/ports
properties:
port@0:
$ref: /schemas/graph.yaml#/properties/port
description:
DSI input port node, connected to the ltdc rgb output port.
port@1:
$ref: /schemas/graph.yaml#/properties/port
description:
DSI output port node, connected to a panel or a bridge input port"
***************************************
Kind regards,
Erwan.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.