2022-07-01 6:28 AM
Hi, the image provided by ST, usb0 ethernet show up as well when try 'ifconfig'.
We would like to try with buildroot.
We pick kernel from ST: linux-5.15-stm32mp-r1.tar.gz
We pick config from ST: en.SOURCES-stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15.tar.xz (inside the zip has config-5.15.24.txt file)
Building and boot are success.
We expected to see "usb_gadget" in folder /sys/kernel/config to run "stm32_usbotg_eth_config.sh". But "usb_gadget" folder doesn't appear.
But we tried:
```
mkdir -p /config
mount -t configfs none /config
```
"usb_gadget" does appear inside /config as well.
So, we change path in script "stm32_usbotg_eth_config.sh", instead of "/sys/kernel/config/usb_gadget" become "/config/usb_gadget".
Script run look fine but all we see just:
[ 45.084215] using random self ethernet address
[ 45.087218] using random host ethernet address
Anyone know what we are missing or any hint?
And why "usb_gadget" only appears when use mount, instead of default "/sys/kernel/config/usb_gadget"?
Many thanks
Note: libcomposite is builtin module but for sure we also tried cmd:
```
modprobe libcomposite
```
2022-09-09 10:01 AM
Hi Dat Tran (Community Member)
Sorry this post is quite old. Did you manage to find a solution to this issue? or maybe in Bootlin community?
https://bootlin.com/blog/building-a-linux-system-for-the-stm32mp1-basic-system/
2022-09-13 6:25 AM
Hi OlivierK, I got it working very well. Thanks a lot.
By the way, do you know STM32H7 (STM32H743) support usb gadget ethernet?
I see somewhere STM32F7 does, I guess STM32H7 support this feature as well but I am not sure.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.