2022-11-10 3:11 AM
Hi all!
I am testing the audio configuration for the stm32mp156C-Dk2, with lastest demo(4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15).
I followed the sound card configuration [tutorial](https://wiki.st.com/stm32mpu/wiki/Soundcard_configuration) and I can't configurate correctly somes controls.
E.g (Analog Playback Volume)
root@stm32mp1:~# amixer -c STM32MP15DK cset name='Analog Playback Volume' '204','204'
amixer: Control sysdefault:0 element write error: Invalid argument
root@stm32mp1:~# amixer -c STM32MP15DK cset name='Analog Playback Volume' '100','100'
numid=3,iface=MIXER,name='Analog Playback Volume'
; type=INTEGER,access=rw---R--,values=2,min=0,max=228,step=0
: values=100,100
| dBscale-min=-102.00dB,step=0.50dB,mute=0In this case, the max argument is 228 but when I try it with the value 204, it says: "invalid argument" but with other lower value it works...
This also happen with others controls.
What is the reason for this to happen?
Regards!
Thanks!
Solved! Go to Solution.
2022-11-29 1:48 AM
This is actually a bug that was introduced in the upstream kernel, in commit 4f1e50d6a9cf9c1b8c859d449b5031cacfa8404e ("ASoC: ops: Reject out of bounds values in snd_soc_put_volsw_sx()"). The problem is described in this thread: https://lore.kernel.org/all/Yph8C3bRxcr6ogW7@sirena.org.uk/T/
The following patch should fix it:
https://lore.kernel.org/all/20220511134137.169575-1-broonie@kernel.org/
Note, that patch series also has an additional patch to apply bounds checking to the second channel:
https://lore.kernel.org/all/20220511134137.169575-2-broonie@kernel.org/
That 2nd channel patch is broken; if you apply it, make sure to also apply this fix:
https://lore.kernel.org/all/20221125162348.1288005-1-ckeepax@opensource.cirrus.com/
Guillermo
2022-11-29 1:48 AM
This is actually a bug that was introduced in the upstream kernel, in commit 4f1e50d6a9cf9c1b8c859d449b5031cacfa8404e ("ASoC: ops: Reject out of bounds values in snd_soc_put_volsw_sx()"). The problem is described in this thread: https://lore.kernel.org/all/Yph8C3bRxcr6ogW7@sirena.org.uk/T/
The following patch should fix it:
https://lore.kernel.org/all/20220511134137.169575-1-broonie@kernel.org/
Note, that patch series also has an additional patch to apply bounds checking to the second channel:
https://lore.kernel.org/all/20220511134137.169575-2-broonie@kernel.org/
That 2nd channel patch is broken; if you apply it, make sure to also apply this fix:
https://lore.kernel.org/all/20221125162348.1288005-1-ckeepax@opensource.cirrus.com/
Guillermo
2022-11-29 2:05 AM
Additionally, if your kernel has this patch applied:
https://lore.kernel.org/all/20220602162119.3393857-7-ckeepax@opensource.cirrus.com/
This is wrong and breaks the volume range for the "PGA Volume" control. The following patch reverts this:
https://lore.kernel.org/all/20221125163748.1288942-2-ckeepax@opensource.cirrus.com/
Full discussion here:
https://lore.kernel.org/all/20221128171622.GI105268@ediswmail.ad.cirrus.com/
Guillermo
2022-11-29 8:46 AM
Thanks @Grodriguez , this solves the problem completely.
I hope they will integrate these patches in a future release.
Cheers.
Alejandro.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.