2021-01-04 5:38 AM
Hi All,
In STM32MP1, i have following two problem related RTC
1. Kernel space
RTC is working fine for me only when i enter following command at every power up , else the default RTC date show local time.
hwclock --localtime --hctosys-- makes RTC works.
root@mp1som:~# date
Mon Sep 7 06:16:00 UTC 2020
root@mp1som:~# hwclock --localtime --hctosys
root@mp1som:~# date
Mon May 26 11:22:49 UTC 2014
2 , Uboot side always shows default RTC time. why this ?
following is uboot log:
U-Boot SPL 2018.11-stm32mp-r3 (Dec 18 2020 - 10:05:24 +0000)
Model: STMicroelectronics STM32MP157A-DK1 Discovery Board
RAM: DDR3-DDR3L 32bits 533000Khz
Trying to boot from MMC1
U-Boot 2018.11-stm32mp-r3 (Dec 18 2020 - 10:05:24 +0000)
CPU: STM32MP157CAA Rev.B
Model: STMicroelectronics STM32MP157A-DK1 Discovery Board
Board: stm32mp1 in basic mode (st,stm32mp157a-dk1)
2021-01-05 5:36 AM
Hi @Ara.1 ,
I read "U-Boot SPL 2018.11-stm32mp-r3" which make me think you are trying to use "basic boot" mode on old V1.2 ecosystem.
Is it on purpose ?
You may be aware that this basic boot scheme is not recommended and even deprecated in V2.x version.
If not already done please read https://wiki.st.com/stm32mpu-ecosystem-v1/wiki/Boot_chains_overview#STM32MP_boot_chains
and related comment about basic.
I also read "root@mp1som".
I you confirm you are using a part from SOM maker integrating STM32MP1, please be aware that the SOM maker is your first and main support contact.
Olivier
2021-01-05 11:00 AM
Hi
its working now.
as the distro uses default system time than local time.
this works by using
hwclock -s
at every power up
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.