2021-11-29 6:07 AM
Hello,
I want to persist data in flash memory from the Cortex M4 program.
I created a section in the linker file:
.mySection 0x000000001002f000 :
{
KEEP(*(.mySection))
} >RAM1_dataSo i know where my data is in the RAM memory but i don't know how to write this data in flash memory so it can be persisted.
I saw a lot of examples for other STM products that use function similar to this:
void Write_Flash(uint8_t data)
{
HAL_FLASH_Unlock();
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR | FLASH_FLAG_PGSERR );
FLASH_Erase_Sector(FLASH_SECTOR_6, VOLTAGE_RANGE_3);
HAL_FLASH_Program(TYPEPROGRAM_WORD, FlashAddress, data);
HAL_FLASH_Lock();
}But i can't find the HAL library containing HAL_FLASH_XXXX function for the STM32mp1 series... Does this library exists?
How can i save the data in the flash memory or somewhere that is persisted after a hardware reboot?
Do i need to transfert data from M4 Core to A7 Core or does another solution exists for the STM32mp1 series? (i prefer to avoid to transfert data between the 2 core)
Best regards,
Ludovic Feltz.
2021-11-29 7:18 AM
Hi @Ludovic Feltz ,
There is NO embedded flash in stm32mp1 and MCURAM is not persistent.
Only persistent storage would be the backup RAM if you power VBAT, or an external flash storage.
Hope it help,
Olivier
2021-11-29 7:22 AM
Hi @Community member
I saw in the linker file the following section:
/* Memories definition */
MEMORY
{
RETRAM_interrupts (xrw) : ORIGIN = 0x00000000, LENGTH = 0x00000298
FLASH_text (rx) : ORIGIN = 0x10000000, LENGTH = 128K
RAM1_data (xrw) : ORIGIN = 0x10020000, LENGTH = 128K
RAM2_ipc_shm (xrw) : ORIGIN = 0x10040000, LENGTH = 0x00008000
}Isn't the FLASH_text memory a flash memory that can be used to persist data?
So you are telling me that i should transfert data to the A7 core and save theses data in the SD Card?
Or can i access SD Card from the M4 Core?
2021-11-29 7:51 AM
Hi @Ludovic Feltz
Where did you get this linker script ?
The one from template delivered in Cube 1.4 looks like this :
MEMORY
{
m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000298
m_text (RX) : ORIGIN = 0x10000000, LENGTH = 0x00020000
m_data (RW) : ORIGIN = 0x10020000, LENGTH = 0x00020000
m_ipc_shm (RW) : ORIGIN = 0x10040000, LENGTH = 0x00008000
}
Anyway, reference to FLASH is probably legacy from MCU kept by mistake.
Storage inside an SDCard drive on A7 side is indeed an option.
You can also directly access to a mass storage device M4 side through sdmmc3, QSPI or FMC interfaces.
Else, M4 can access directly to Backup RAM, taking care begin of this area is used by OpenSTLinux for low power management.
Olivier
2021-11-29 7:59 AM
@Community member
Thank you for your quick response.
I use STM32CubeMX version 6.3.0 to generate the code (and so the linker script).
Ok i will try to find a way using sdmmc3 and reading some documentation about backup RAM. (is the creation of a section possible as with the normal RAM?)
2024-02-21 8:38 AM - edited 2024-02-21 8:39 AM
@Olivier GALLIEN wrote:Storage inside an SDCard drive on A7 side is indeed an option.
You can also directly access to a mass storage device M4 side through sdmmc3, QSPI or FMC interfaces.
I guess it is not possible to share one flash device (SD or eMMC) by both the A7 and M4 cores. I can't imagine how this could possibly work and how both cores would synchronize access to the device. Definitely shouldn't work with QSPI as one slave device cannot be accessed by multiple master devices at the same time.
In other words, if you already have a Linux running on your A7 and being in control of the SD or eMMC, the only chance to store data persistently from the firmware running on the M4 is to have some user-space daemon in Linux-land taking care of it, communicating via OpenAMP. Am I right?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.