2020-09-15 12:04 PM
Hi everyone,
STM32MP1 ROM Code has default AF mux for SPI_NOR/NAND like this:
QUADSPI_CLK -> PF10 (AF9)
QUADSPI_BK1_NCS -> PB6 (AF10)
QUADSPI_BK1_IO0 -> PF8 (AF10)
QUADSPI_BK1_IO1 -> PF9 (AF10)
I want to remap to the new pins using the OTP CFG5..7
The poinst is, what is the order of usage.
Which part of which word should be assigned to which function.
My used pins like this:
QUADSPI_CLK -> PG7 (AF9)
QUADSPI_BK1_NCS -> PB10 (AF9)
QUADSPI_BK1_IO0 -> PD11 (AF9)
QUADSPI_BK1_IO1 -> PF9 (AF10)
so how should be seen the OTG Word 5 .. 7? My decision is like that. but i want to make sure it is true.
CFG5: 0x77912A97
CFG6: 0x4B9169A1
Solved! Go to Solution.
2020-09-16 6:08 AM
Hello @tmkaran ,
You reverted CFG5 and CFG6 order, it should be like this:
CFG5: 0x2A97 7791
CFG6: 0x69A1 4B91
Else it seems correct. Don't forget to set to 1 in the word3 the parameter qspi_not_default_af.
Armand
2020-09-16 6:08 AM
Hello @tmkaran ,
You reverted CFG5 and CFG6 order, it should be like this:
CFG5: 0x2A97 7791
CFG6: 0x69A1 4B91
Else it seems correct. Don't forget to set to 1 in the word3 the parameter qspi_not_default_af.
Armand
2020-09-16 8:51 AM
Thank you very much @ArmandG. It works!
tmk
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.