2019-10-15 6:42 AM
Hi,
I wanted to flash the EVAL board with the latest Android version and I've got this error (see attached file)
Any idea ?
Thanks !
Best regrads,
Anthony Harivel
2019-10-15 9:23 AM
Hi,
As far as I understood, you want to flash the images on the embedded emmc. For that purpose, you should use the FlashLayout_emmc_optee.tsv file. The clear is only to reset the emmc as Android can't be flashed on emmc and on sdcard at the same time (conflict between partitions with the same name).
Regards
Nicolas
2019-10-16 12:01 AM
Hi Nicolas,
Well I don't really understand what I'm doing wrong. Because I'm using the EVAL board, I've got the ST-Link USB (CN4) connected, the USB OTG (CN16) connected, the BOOT pin are on OFF (DFU), and JP4, JP5 so that the serial goes to the ST-LINK.
I just want to flash the eMMC and I've downloaded this "st-android-9.0.0-2019-09-27-eval-emmc-starter". There is 2 TSV files: the "..._clear.tsv" and the "..._optee.tsv",
Both give me the same result as above..
Any idea?
Thanks,
Regards
Anthony
2019-10-16 2:31 AM
Hi
What is strange is that your SN is 0000000. What is the version of your board ?
Regards
Nicolas
2019-10-16 5:55 AM
Hi
I don't know which number to give ? this one : MB1263B-04 ?
Regards
Anthony
2019-10-16 6:03 AM
Hi
This this the number I expected. It confirms that your board has been provided through specific partner program. It is no more supported (old version).
I suggest you to contact your official contact to exchange your board with the latest one. You must have a MB1263C board.
Regards
Nicolas
2019-10-16 6:12 AM
Hi
Oh right ! oups.. ok well I'll ask to exchange the board!
Thank you for your prompt answer !
Regards
Anthony
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.