2021-09-23 9:06 PM
Hi,
My evaluation kit is stm32mp157c-ev1, I can flash code to eMMC or SD via STM32CubeProgrammer successfully, and it can work expectedly.
We need to running program on eMMC without SD card. Flash the eMMC code via STM32CubeProgrammer is very slow and is not suitable for mass production.
Please support a script that flash eMMC code "stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31" via SD card.
Thanks,
QiZhang
2021-09-27 1:21 AM
Hi @zqizh.1 ,
Please have a look to post
https://community.st.com/s/question/0D50X0000BiBhHQSQ0/stm32mp153a-failed-to-boot-from-emmc
It contain a guide to load eMMC from SDcard with Uboot.
Does it suit your need ?
Olivier
2021-09-27 1:46 AM
Hi Olivier,
Your solution is not I want.
Below script is I got from internet to write the image to eMMC card from SD card.
But I don't know how to create eMMC image "atk_emmc-stm32mp157d-atk-qt.raw".
Your distribution package include a script "create_sdcard_from_flashlayout.sh" which can generate a SD card image, Please support a similar script to generate a eMMC image for me.
Thanks,
QiZhang
"
echo "enable eMMC write flag"
echo 0 > /sys/class/block/mmcblk1boot0/force_ro
echo 0 > /sys/class/block/mmcblk1boot1/force_ro
echo "flashing tf-a,please wait..."
execute "dd if=./tf-a/tf-a-stm32mp157d-atk-trusted.stm32 of=${device}boot0 conv=fsync"
execute "dd if=./tf-a/tf-a-stm32mp157d-atk-trusted.stm32 of=${device}boot1 conv=fsync"
echo "close eMMC write flag"
echo 1 > /sys/class/block/mmcblk1boot0/force_ro
echo 1 > /sys/class/block/mmcblk1boot1/force_ro
execute "mmc bootpart enable 1 1 ${device}"
echo "flashing bootfs and rootfs,please wait..."
execute "dd if=./atk_emmc-stm32mp157d-atk-qt.raw of=${device} bs=8M conv=sync status=progress"
echo "partition..."
sgdisk -d 3 ${device}
sync
sgdisk -a 1 -n 3:136192:0 -c 3:rootfs -t 3:8300 -u 3:491f6117-415d-4f53-88c9-6e0de54deac6 ${device}
sync
echo "eMMC flash completed�?"
"
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.