2021-01-21 11:02 PM
Hi ST.
I set the clock in the dts file as below.
&rcc {
st,hsi-cal;
st,csi-cal;
st,cal-sec = <60>;
st,clksrc = <
CLK_MPU_PLL1P
CLK_AXI_PLL2P
CLK_MCU_PLL3P
CLK_PLL12_HSE
CLK_PLL3_HSE
CLK_PLL4_HSE
CLK_RTC_LSE
CLK_MCO1_DISABLED
CLK_MCO2_DISABLED
>;
st,clkdiv = <
1 /*MPU*/
0 /*AXI*/
0 /*MCU*/
1 /*APB1*/
1 /*APB2*/
1 /*APB3*/
1 /*APB4*/
2 /*APB5*/
23 /*RTC*/
0 /*MCO1*/
0 /*MCO2*/
>;
st,pkcs = <
CLK_CKPER_HSI
CLK_QSPI_ACLK
CLK_ETH_DISABLED
CLK_SDMMC12_PLL4P
CLK_STGEN_HSE
CLK_USBPHY_HSE
CLK_SPI2S1_CKPER
CLK_SPI2S23_PLL3Q
CLK_SPI45_PLL4Q
CLK_SPI6_DISABLED
CLK_I2C46_HSI
CLK_SDMMC3_DISABLED
CLK_USBO_USBPHY
CLK_ADC_PLL4R
CLK_CEC_DISABLED
CLK_I2C12_HSI
CLK_I2C35_DISABLED
CLK_UART1_HSI
CLK_UART24_HSI
CLK_UART35_HSI
CLK_UART6_HSI
CLK_UART78_HSI
CLK_SPDIF_DISABLED
CLK_SAI1_DISABLED
CLK_SAI2_DISABLED
CLK_SAI3_DISABLED
CLK_SAI4_DISABLED
CLK_RNG1_LSI
CLK_RNG2_LSI
CLK_LPTIM1_PCLK1
CLK_LPTIM23_PCLK3
CLK_LPTIM45_LSE
>;
/* VCO = 1066.0 MHz => P = 266 (AXI), Q = 533 (GPU), R = 533 (DDR) */
pll2: st,pll@1 {
compatible = "st,stm32mp1-pll";
reg = <1>;
cfg = < 2 65 1 1 0 PQR(1,0,1) >;
frac = <0x1400>;
};
/* VCO = 600.0 MHz => P = 200, Q = 40, R = 60 */
pll3: st,pll@2 {
compatible = "st,stm32mp1-pll";
reg = <2>;
cfg = < 3 99 2 14 9 PQR(1,1,1) >;
/*
frac = <0x1a04>;
*/
};
/* VCO = 792.0 MHz => P = 99, Q = 66, R = 72 */
pll4: st,pll@3 {
compatible = "st,stm32mp1-pll";
reg = <3>;
cfg = < 5 197 7 11 10 PQR(1,1,1) >;
};
};
The following is the SPI setting part of M4 Core Side.
static void MX_SPI5_Init(void)
{
LL_SPI_InitTypeDef SPI_InitStruct = {0};
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
if (IS_ENGINEERING_BOOT_MODE())
{
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_SPI45;
PeriphClkInit.Spi45ClockSelection = RCC_SPI45CLKSOURCE_PLL4;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
}
else
{
if (!LL_RCC_PLL4_IsReady())
{
LL_RCC_PLL4_Enable();
}
LL_RCC_PLL4Q_Enable();
}
// Peripheral clock enable
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SPI5);
LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOK);
LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOJ);
/* SPI5 GPIO Configuration
PK0 ------> SPI5_SCK
PJ10 ------> SPI5_MOSI
*/
GPIO_InitStruct.Pin = LL_GPIO_PIN_0;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_MEDIUM;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
GPIO_InitStruct.Alternate = LL_GPIO_AF_5;
LL_GPIO_Init(GPIOK, &GPIO_InitStruct);`
GPIO_InitStruct.Pin = LL_GPIO_PIN_10;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_MEDIUM;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
GPIO_InitStruct.Alternate = LL_GPIO_AF_5;
LL_GPIO_Init(GPIOJ, &GPIO_InitStruct);
SPI_InitStruct.TransferDirection = LL_SPI_SIMPLEX_TX;
SPI_InitStruct.Mode = LL_SPI_MODE_MASTER;
SPI_InitStruct.DataWidth = LL_SPI_DATAWIDTH_16BIT;
SPI_InitStruct.ClockPolarity = LL_SPI_POLARITY_LOW;
SPI_InitStruct.ClockPhase = LL_SPI_PHASE_1EDGE;
SPI_InitStruct.NSS = LL_SPI_NSS_SOFT;
SPI_InitStruct.BaudRate = LL_SPI_BAUDRATEPRESCALER_DIV2;
SPI_InitStruct.BitOrder = LL_SPI_MSB_FIRST;
SPI_InitStruct.CRCCalculation = LL_SPI_CRCCALCULATION_DISABLE;
SPI_InitStruct.CRCPoly = 0x0;
LL_SPI_Init(SPI5, &SPI_InitStruct);
LL_SPI_SetStandard(SPI5, LL_SPI_PROTOCOL_MOTOROLA);
}
The following is the part that transmits data using SPI in M4 Core Side.
uint16_t uData = 0xFF0F;
LL_SPI_SetTransferSize(SPI5, 1);
LL_SPI_Enable(SPI5);
LL_SPI_StartMasterTransfer(SPI5);
LL_SPI_TransmitData16(SPI5, uData);
while (LL_SPI_IsActiveFlag_EOT(SPI5) == 0);
LL_SPI_ClearFlag_EOT(SPI5);
LL_SPI_ClearFlag_TXTF(SPI5);
LL_SPI_SuspendMasterTransfer(SPI5);
LL_SPI_Disable(SPI5);
SPI5 uses PLL4Q.
PLL4Q = 66Mhz -> 66/2 -> 33Mhz
The clock of SPI5 should operate at 33Mhz, but as a result of checking with an actual oscilloscope, it is about 2.6Mhz.
When I check it with an oscilloscope in Engineering Mode, it is about 33Mhz, but it is 2.6Mhz in Production Mode (Linux).
Am I wrong clock or SPI5 settings?
Below is the development environment.
Board : Custom board using stm32mp151c chip.
OS : Ecosystem 2.1.0 (202-11-12)
IDE : STM32CubeIDE
Debugger : STLINK-V3SET
Please tell me a solution.
Regards
Machilus
Solved! Go to Solution.
2021-02-10 10:33 AM
Hi Machilus (Community Member),
There should be no influence at all of M4 clock init code in production mode since all the clock settings are initialized exclusively by the Linux DT in production mode. Mixing M4 code calling RCC clock setting such as the prescaler is conflicting with openstlinux RCC init in DT.
Therefore this LL_SPI_BAUDRATEPRESCALER_DIV2 may work in engineering mode where the M4 is isolated from the Cortex A7 and Linux, but not in production mode.
So I would strip out first all the RCC code settings from the M4, regenerate/reload the .elf file. Refer to the CubeMX code generator tool to generate the clock tree (including the clock prescalers) in production mode and see how it goes.
you can refer to the wiki ressources for that if not clear:
Regards,
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.