2022-03-11 5:43 AM
Hello
I created own machine based of seeed module.
at the strartup there is info
NOTICE: CPU: STM32MP157CAC Rev.B
NOTICE: Model: STMicroelectronics custom STM32CubeMX board - openstlinux-5.10-dunfell-mp1-21-03-31
WARNING: VDD unknown
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe3000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.4-r1.0(debug):v2.4-dirty
NOTICE: BL2: Built : 16:43:51, Nov 17 2020
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000kHz
WARNING: Couldn't find property st,phy-cal in dtb
ERROR: DDR addr bus test: can't access memory @ 0xc0000004
PANIC at PC : 0x2ffedb39
Exception mode=0x00000016 at: 0x2ffedb39I'm pretty new in linux on low lvl. Do anyone know where should i look for mistakes? Hardware is ok, i checked it on official image.
2022-03-14 7:44 AM
Hello TStas.2 (Community Member)
When you say you checked the h/w on official image, then you can boot normally?
Otherwise it be worth looking at this article for exploring DDR issues.
STM32MP1 bring-up troubleshooting guide
FAQ: STM32MP1 how to validate the STM32MP1-DRAM connection on PCB, DDR test suite
Rgds,
Olivier
2022-03-14 8:12 AM
Yes i mean that all works ok
But i see
-Check configuration I2Cbus connection to STPMIC
I2C bus for pmic is done at early phase and raises a panic when the bus fails to be enabled.
In OpenSTLinux by default, TF-A expects STPMIC on I2C4. If this is not the case on your design device tree and TF-A code have to be modified.In fact STPMIC is connected to I2C2. Maybe it will be solution. Tomorow i will check it. Thank You
2022-03-23 2:31 AM
Hi TStas.2 (Community Member)
Any progress with this issue? I guess you've already made the changes in TF-A regarding I2C2?
Regards,
Olivier
2022-03-23 3:24 AM
meanwhile i had different tasks, so i didn't focus 100% on that. But after changes i Have still some problem. Now i tryind test it step by step and compare with refference files.
/PANIC at PC : 0x2fff08eb
Exception mode=0x00000016 at: 0x2fff08eb
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.