2024-05-02 10:52 AM
Hello,
I am currently using the MOOC hands-on lab examples to understand how to use inter processor communication between the A7 and M4. The lab is using the STM32MP157C-DK2 board, whereas I am using the STM32MP157F-DK2 board.
Currently, I made a new CubeMX project for the STM32MP157F-DK2 board and tried to import the lab example project to into the new project but the import project option is grayed out in CubeMX. How can I port the inter processor lab examples to run on the STM32MP157F-DK2 board using STM32CubeMX? I appreciate any help with this, thank you.
2024-05-03 5:46 AM
Hi @daded.1 ,
This is actually not fast forward since MOOC has been published long time ago with the first ecosystem.
I recommand you to use latest ecosystem for both OpenSTLinux and all tools ( CubeMX).
I guess reading and following FAQ : STM32MP1 – How to migrate STM32CubeMx projec... - STMicroelectronics Community may helps.
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.