STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP15 ECO 5.0.0. kernel halts after Secondary CPU 1 switching to normal world boot

Custom board. Boot log as belowextlinux.conf:MENU BACKGROUND /splash_landscape.bmpTIMEOUT 20LABEL OpenSTLinuxKERNEL /uImageFDTDIR /INITRD /st-image-resize-initrdAPPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=${console},...

Resolved! STM32MP157 - memory for the M4 core

Dear experts. ​we plan to use a STM32MP157, where the A7 core should have 512MB DDR RAM, and theM4 core 16 MB. What options exists, to give the M4 core that 16 MB of RAM?From the DS, i understand that the DDR RAM of the A7 is not accessible for the M...

Resolved! OPTEE backwards compatibility

Hi,We are using the meta-st-stm32mp layer in out Yocto build system. We have had the system run on the Dunfell distribution up until now with OPTEE as the secure OS.For Dunfell the version of OPTEE is 3.12 along with patches from ST, a we tried to up...

Resolved! STM32MP157C-DK2 fails to load system to SD

Good. I am trying to load the system to my stm32mp157c-dk2 using STM32CubeProgrammer software, but I get the same error when loading partition 13 every time. The error is as follows: Error: failed to download Segment[0] Error: failed to download the ...

Magnoacd by Associate II
  • 4669 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.