2019-09-26 8:02 AM
Hello,
I'm using the OpenAMP_TTY_echo example with some modification.
if (VirtUart0RxMsg) {
VirtUart0RxMsg = RESET;
while (data < 65535) {
itoa(data, buf, 10);
if(VIRT_UART_Transmit(&huart0, (uint8_t *)buf, 10) != VIRT_UART_OK){
Error_Handler();
}
data ++;
}
data = 0;
}On Linux side I'm use write on ttyRPMSG0.
But if I don't read, the log give me the message:
rpmsg_tty virtio0.rpmsg-tty-channel.-1.0: No memory for tty_prepare_flip_string
I think that I'm understand the problem, but what can I do to prevent this problem?
Solved! Go to Solution.
2019-10-25 7:26 AM
Hello @lenonrt,
Regarding the "No memory for tty_prepare_flip_string" message the bottleneck seems to be your application... A lot of root causes can explain your issue which probably depends on the other tasks the processor executes.
Regarding the code you shared, you Rpmsg are filled with only 10- bytes. Each message generates an interruption on Cortex-A7, this is not optimum. I would suggest to concatenate the buffers to fill the whole RPMsg buffer which can contain up to 496 bytes (by default). With this optimization you should significantly decrease the number of mailbox (IPCC) interruptions.
Now If you are looking for an alternative based on separate shared buffers you can have a look here: https://github.com/STMicroelectronics/meta-st-stm32mpu-app-logicanalyser
This sample is relying on a rpmsg_sdb Linux drivers which allows to to expose buffers to userland. the RPMsg is used to provide the buffer addresses to the Cortex-M4 which inform the Cortex-A7 when a buffer is filled.
Be aware that the rpmsg_sdb driver is provided only as example implementing transfer from Cortex-M4 to Cortex-A7. You can use it as a guide to implement your own driver.
Arnaud
2019-09-27 7:17 AM
Hi @lenonrt
I understand you are not reading the message you sent on A7 side.
So I guess you reach the queue message or buffer full
Try to implement a process on A7 reading the message.
Olivier
2019-10-17 7:16 AM
Hi @Community member , thank you for your answer!
Yes, you are right.
I was trying to use for sending data. I try to receive the messages on A7.
But after some seconds the problem occurs again.
I do some tests with a 496 bytes buffer message using request and answer method.
I get 18Mb/s which isn't a good. I saw in the forum that you say ST achieved 15.4MB/s.
Now I'm developing to send just a pointer.
Lenon
2019-10-25 7:26 AM
Hello @lenonrt,
Regarding the "No memory for tty_prepare_flip_string" message the bottleneck seems to be your application... A lot of root causes can explain your issue which probably depends on the other tasks the processor executes.
Regarding the code you shared, you Rpmsg are filled with only 10- bytes. Each message generates an interruption on Cortex-A7, this is not optimum. I would suggest to concatenate the buffers to fill the whole RPMsg buffer which can contain up to 496 bytes (by default). With this optimization you should significantly decrease the number of mailbox (IPCC) interruptions.
Now If you are looking for an alternative based on separate shared buffers you can have a look here: https://github.com/STMicroelectronics/meta-st-stm32mpu-app-logicanalyser
This sample is relying on a rpmsg_sdb Linux drivers which allows to to expose buffers to userland. the RPMsg is used to provide the buffer addresses to the Cortex-M4 which inform the Cortex-A7 when a buffer is filled.
Be aware that the rpmsg_sdb driver is provided only as example implementing transfer from Cortex-M4 to Cortex-A7. You can use it as a guide to implement your own driver.
Arnaud
2019-10-25 10:23 AM
Hello,
Thanks for the information!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.