2020-11-05 6:06 PM
when i using a 100M network cable in a gigabit network,It should be recognized as a 100M network under normal circumstances,But STM32MP1 is recognized as Gigabit,at this time the network is useless,led is light but not blink,I changing cable to a Gigabit Ethernet cable solved the problem,I am using stm32mp157c-dk2
Solved! Go to Solution.
2020-11-23 11:42 PM
This is confirmed as a regression on the Realtek RTL8211F community driver for kernel 5.4.
RTL8211E used on STM32MP157x-EV1 is not affected.
This is not related to ST work (although we should have discovered this regression), we are checking for a patch or a solution.
I keep you posted if I see progress.
Regards.
2020-11-09 2:48 AM
Hello,
a similar issue is under analysis internally. I will make an update when I get feedback.
2020-11-23 11:42 PM
This is confirmed as a regression on the Realtek RTL8211F community driver for kernel 5.4.
RTL8211E used on STM32MP157x-EV1 is not affected.
This is not related to ST work (although we should have discovered this regression), we are checking for a patch or a solution.
I keep you posted if I see progress.
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.