2025-11-25 3:21 AM
Hi I was trying to connect a custom LVDS display to my STM32MP257F-dk board but it does not seem to work,
The display has a resolution of 1024x600 pixel and also it uses "vesa-24" scheme, so i assume that i don't need to change the device tree as it matches the specification of the default display which is supplied with the dev kit. If otherwise please advice.
Please not that i am not using the touch panel of the display so the i2c connection of the dev kit are not connected to the display board can that disable the LVDS port ?
Is there any way to debug the LVDS display, Please advise in this matter.
Regards,
Samip
2025-12-05 11:26 PM
Hey can anyone help on this ?? I was hoping to get a reply.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.