2023-03-02 7:53 AM
STM32MP135 is connect on i2c bus to 3 devices:
I am using linux kernel 5.15.24 synched with your github repo. LM75 and PCF8563 are working fine. INA233 has problems to manage the PEC (Packet Error Correction)
I am seeing lot of this errors:
stm32f7-i2c 40012000.i2c: Bad PEC 0x89 vs. 0x79
stm32f7-i2c 40012000.i2c: Bad PEC 0x89 vs. 0xc7
stm32f7-i2c 40012000.i2c: Bad PEC 0x89 vs. 0xed
I checked on the st driver that the PECEN is flagged since the i2c slave device has the PEC capability, and I am receving the PEC fo=rom the device in the log: 0x79, 0xcf, 0xed.
The strange think is that the register value read from stm device is always 0x89.
This value is read using the
internal_pec = readl_relaxed(i2c_dev->base + STM32F7_I2C_PECR)
It seems the register is not properly updated.
Any idea or suggestion?
2023-09-28 7:38 AM
Could you please test this patch ? (it is based on kernel 6.10)
---
drivers/i2c/busses/i2c-stm32f7.c | 9 ++++++---
1 file changed, 6 insertions(+), 3 deletions(-)
diff --git a/drivers/i2c/busses/i2c-stm32f7.c b/drivers/i2c/busses/i2c-stm32f7.c
index 97f7aced4f07..ff33a5e3e6e7 100644
--- a/drivers/i2c/busses/i2c-stm32f7.c
+++ b/drivers/i2c/busses/i2c-stm32f7.c
@@ -1071,9 +1071,10 @@ static int stm32f7_i2c_smbus_xfer_msg(struct stm32f7_i2c_dev *i2c_dev,
/* Configure PEC */
if ((flags & I2C_CLIENT_PEC) && f7_msg->size != I2C_SMBUS_QUICK) {
cr1 |= STM32F7_I2C_CR1_PECEN;
- cr2 |= STM32F7_I2C_CR2_PECBYTE;
- if (!f7_msg->read_write)
+ if (!f7_msg->read_write) {
+ cr2 |= STM32F7_I2C_CR2_PECBYTE;
f7_msg->count++;
+ }
} else {
cr1 &= ~STM32F7_I2C_CR1_PECEN;
cr2 &= ~STM32F7_I2C_CR2_PECBYTE;
@@ -1161,8 +1162,10 @@ static void stm32f7_i2c_smbus_rep_start(struct stm32f7_i2c_dev *i2c_dev)
f7_msg->stop = true;
/* Add one byte for PEC if needed */
- if (cr1 & STM32F7_I2C_CR1_PECEN)
+ if (cr1 & STM32F7_I2C_CR1_PECEN) {
+ cr2 |= STM32F7_I2C_CR2_PECBYTE;
f7_msg->count++;
+ }
/* Set number of bytes to be transferred */
cr2 &= ~(STM32F7_I2C_CR2_NBYTES_MASK);
--
2.25.1
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.