2021-12-15 12:59 AM
Hello,
I am working on IPC between M4 and A7 and it works properly using the "logic analyzer" example. I changed it according to my needs but not the buffers.
1 . I could read the data from 3 buffers, but often buffers are swapping. I would like to what causes this problem and how to solve it?
2. When I start IPC, one of the CPU processes goes into 100%. Is it normal for the IPC? and is there anything that I could change to reduce the CPU processes?
Thank you in advance
2021-12-16 6:50 AM
Hi @JSIGA.1 ,
Can you please provide some more context ?
Which OpenSTLinux version ?
Custom or ST board ?
I understand that default logic analyze was working properly and reported issues comes only with your 'changed it according to my needs' right ?
Could you share details of those changes ?
Thx
Olivier
2021-12-17 1:13 AM
Hello Olivier,
I have a custom board which is based on stm32mp157A.
I am using openSTLinux Dunfell but i don't know which version exactly.
I am trying to send around 50kilobytes of data with frame numbers for every buffer from M4 to A7 in every 100ms. I have not touched the Sending part in logic analyze code of M4.
In A7, I haven't touched the reading part . When the buffer filled event occurred, I read the data and process those. (processing time of the 50kb data is 8 milliseconds in A7)
I am successfully reading the data without any frame loss or frame swapping from A7 for around 15 minutes. after that, the buffer swapping problem arises for a couple of buffers and disappeared, again in the next 2 or 3 mins, it appears again and disappeared.
Regarding my second question, I found a small bug in my code, which consumes a lot of CPU resources. after changing that the CPU usage has been reduced. but still, I have a buffer swapping problem.
JS
2021-12-20 2:13 AM
Hi @JSIGA.1 ,
No evidence here.
I guess it deserve a careful system debug to try to catch the root cause.
Anyway, maybe one clue to evacuate would be a potential cache coherency issue as per already faced in this post :
https://community.st.com/s/question/0D53W00000uXp2hSAC/rpmsg-sdb-cached-buffer
I attached the recommended patch to apply in rpmsg_sdb driver.
Let us know.
Thx
Olivier
2021-12-21 7:43 AM
Hai,
I have tried changing to DMA coherent, but it didn't help me in my case. Still, the problem persists.
JS
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.