STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Linux device drivers for RTL8211F-CG

Hello. I'm working with STM32MP15-DK1. There is the Realtek IC: RTL8211F-CG. Driver for this IC situates in SDK: linux-5.10.10/drivers/net/phy/realtek.cThere are two defines in this file: #define RTL8211F_TX_DELAY BIT(8)#define RTL8211F_RX_DELAY BIT(...

DFomi.1 by Associate II
  • 6367 Views
  • 1 replies
  • 0 kudos

Resolved! Rootfs size expansion

Hi ,How can i increase the size of rootfs correctly? I tried using gparted , but it looks like the tf-a iss't very happy with it and tries to reset it in correct way. So i would like to understand how can i increase its size more correctly since inst...

NPal.2 by Senior
  • 4377 Views
  • 8 replies
  • 1 kudos

Resolved! Getting started, stuck at building kernel with make ARCH=arm multi_v7_defconfig fragment*.config

Hey guys,Having some issues with running through the kernel setup and dont understand the errors returned back as iv followed all the steps to a T.Attached my terminal history. This in on the https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1...

AMeta by Associate II
  • 9181 Views
  • 2 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.