2022-08-16 12:21 AM
Link to the tutorial and warning:
WARNING: st-image-weston-1.0-r0 do_st_write_license_create_summary: IMG LIC SUM: File does not exist with open file /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp1-test/tmp-glibc/deploy/licenses/st-image-resize-initrd-openstlinux-weston-stm32mp1-test-20220815132043/package.manifest
Solved! Go to Solution.
2022-08-23 9:06 AM
may be this wil help you. it helped me :
2022-08-16 2:53 AM
Hello @Gencay ,
I already saw this kind of error, but I can't find again what was the issue. My best lead is when you used the command
DISTRO=openstlinux-weston MACHINE=<machine> source layers/meta-st/scripts/envsetup.shA license agreement opens. Did you agree with the license agreement?
Regards,
Kevin
2022-08-16 3:05 AM
Yes I agreed first time when it is asked, I just tried again sourcing the environment but agreement did not come up, below output is displayed:
Linux Distrib: Ubuntu
Linux Release: 20.04
Required packages for Linux Distrib:
bsdmainutils build-essential chrpath cpio debianutils diffstat gawk gcc-multilib git iputils-ping libegl1-mesa libgmp-dev libmpc-dev libsdl1.2-dev libssl-dev lz4 pylint python3 python3-git python3-jinja2 python3-pexpect python3-pip socat texinfo unzip wget xterm xz-utils zstd
Check OK: all required packages are installed on host.
[source layers/openembedded-core/oe-init-build-env][with previous config]
===========================================================================
Configuration files have been created for the following configuration:
DISTRO : openstlinux-weston
DISTRO_CODENAME : kirkstone
MACHINE : stm32mp1-test
BB_NUMBER_THREADS : <no-custom-config-set>
PARALLEL_MAKE : <no-custom-config-set>
BUILDDIR : build-openstlinuxweston-stm32mp1-test
DOWNLOAD_DIR : /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/Shared/downloads
SSTATE_DIR : /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/Shared/sstate-cache
SOURCE_MIRROR_URL : <no-custom-config-set>
SSTATE_MIRRORS : <disable>
WITH_EULA_ACCEPTED: YES
===========================================================================
Available images for OpenSTLinux layers are:
- Official OpenSTLinux images:
st-image-weston - OpenSTLinux weston image with basic Wayland support (if enable in distro)
- Other OpenSTLinux images:
- Supported images:
st-image-core - OpenSTLinux core image
You can now run 'bitbake <image>'
2022-08-23 8:34 AM
I have the same issue with the new distro Kirkstone.
My layers working perfect with dunfell.
I made changes for the kirkstine distro and all compiles and i have all the images files but no flashlayouts. :face_with_steam_from_nose:
2022-08-23 9:06 AM
may be this wil help you. it helped me :
2022-08-24 5:02 AM
Thank you so much I will try this one.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.