2026-02-04 4:32 AM
I have used HSEM on STM32H7 very well.
Recently,I test the HSEM of STM32MP257 in development mode, by JTAG/SWD,
I can lock the semaphore by reading the HSEM_RLRx register via CPU1~3,
but after power reset,when I write the HSEM_RLRx register to lock or unlock semaphore, it doesn't work!
the security /privilege / CID filtering of HSEM are all off after reset, and the cpu3 could access the HSEM_RLRx register correctly,but after cpu1/2 write the HSEM_RLRx register or HSEM_CnIER,both lock and unlock operations have no effect.
pls give me some suggestions to check what I might have done wrong .thanks!
2026-02-06 4:15 AM
And why the newest STM32MP21 series has deleted the HSEM module ?
This module is quite useful in multi-core applications.
2026-02-06 8:24 AM
As far as I know, HSEM is inherited from STM32MP15 family but finally not used in STM32MP25 and STM32MP23 software as all our inter-processor communication uses IPCC (also in STM32MP15).
I confirm it has been removed in STM32MP21.
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.