2023-01-10 5:38 AM
The flashing process of our STM32MP1 SoM is very slow, it took about 3 and 1/2 hours to flash to whole 8GB eMMC. We use the STM32_Programmer_CLI and have a usb connection which shows up in DFU mode. How can we speed up the flashing process? How could we debug this? Can we flash multiple devives in parallel?
How we use the STM32_Programmer_CLI ( v2.12) with Ubuntu 22.10:
sudo STM32_Programmer_CLI -c port=USB1 -tm 30000 -w flashlayout_device-image/flashlayout_device.tsvOur tsv file
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl1-boot Binary none 0x0 arm-trusted-firmware/tf-a-phycore-stm32mp1-4-serialboot.stm32
- 0x03 ssbl-boot Binary none 0x0 u-boot/u-boot-phycore-stm32mp1-4-trusted.stm32
P 0x04 fsbl1 Binary mmc1 boot1 arm-trusted-firmware/tf-a-phycore-stm32mp1-4-trusted.stm32
P 0x05 fsbl2 Binary mmc1 boot2 arm-trusted-firmware/tf-a-phycore-stm32mp1-4-trusted.stm32
PD 0x06 ssbl Binary mmc1 0x00080000 u-boot/u-boot-phycore-stm32mp1-4-trusted.stm32
P 0x10 bootA System mmc1 0x00180000 st-image-bootfs-viza-distro-phycore-stm32mp1-4.ext4
P 0x11 bootB System mmc1 0x04180000 st-image-bootfs-viza-distro-phycore-stm32mp1-4.ext4
P 0x20 rootfsA FileSystem mmc1 0x08180000 device-image-phycore-stm32mp1-4.ext4
P 0x21 rootfsB FileSystem mmc1 0xA8180000 device-image-phycore-stm32mp1-4.ext4
P 0x30 paramfs FileSystem mmc1 0x148180000 paramfs.ext4
P 0x32 userfs FileSystem mmc1 0x158180000 datafs.ext4
P 0x31 logfs FileSystem mmc1 0x198180000 logfs.ext4
2023-01-10 8:32 AM
Hi @defqon1
Similar topic than https://community.st.com/s/question/0D53W0000216zGVSAY/stm32mp1-program-few-gb-image-take-too-long
Regards,
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2023-01-10 8:40 AM
Btw, usual CubeProgrammer speed is around 2-3MB/s average, so your 8GB should take less than one hour.
Maybe check that your are not connected using Full-Speed (Board or PC setup or cable or Hub issues).
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.