2022-06-17 2:25 PM
So basically I'm trying to implement WebRTC and seems like aiortc is its python implementation right now:.
Unable to manually install them using pip3 as it requires some dev-packages.
I tried to install it as a layer using pipoe auto-generated recipe, but no luck as it goes on with errors. A working recipe and additions that has to be done to local.conf or CORE_IMAGE_EXTRA_INSTALL variable would be appreciated :smiling_face_with_smiling_eyes:.
Solved! Go to Solution.
2022-06-20 2:59 AM
Hi @Jaison M
This recipe generates a package that I have successfully installed on my board (stm32mp157c-dk2):
DESCRIPTION = "aiortc is a library for Web Real-Time Communication (WebRTC) and \
Object Real-Time Communication (ORTC) in Python."
HOMEPAGE = "https://github.com/aiortc/aiortc"
SECTION = "devel/python"
AUTHOR = "Jeremy Laine"
LICENSE = "BSD"
LIC_FILES_CHKSUM = "file://LICENSE;md5=907b5e856b2e6bcd8a3cc8d338a6166f"
SRC_URI[md5sum] = "3f43e88416113141b0196bdf6c37b444"
SRC_URI[sha256sum] = "15608d7fcf09502d1b8c19b8a63bc22966090ee0761ac9a755e9f747f46d67ab"
PYPI_PACKAGE = "aiortc"
DEPENDS += " \
${PYTHON_PN}-setuptools-scm-native \
${PYTHON_PN}-toml-native \
"
inherit pypi python_setuptools_build_meta
RDEPENDS:${PN} += " \
ffmpeg \
libopus \
libsrtp \
libvpx \
"
BBCLASSEXTEND += "native nativesdk"I did this quick test with the OpenSTLinux distribution that should be released soon. Results may differ against OpenSTLinux ecosystem 3.1
Best regards,
--JM
2022-06-20 2:59 AM
Hi @Jaison M
This recipe generates a package that I have successfully installed on my board (stm32mp157c-dk2):
DESCRIPTION = "aiortc is a library for Web Real-Time Communication (WebRTC) and \
Object Real-Time Communication (ORTC) in Python."
HOMEPAGE = "https://github.com/aiortc/aiortc"
SECTION = "devel/python"
AUTHOR = "Jeremy Laine"
LICENSE = "BSD"
LIC_FILES_CHKSUM = "file://LICENSE;md5=907b5e856b2e6bcd8a3cc8d338a6166f"
SRC_URI[md5sum] = "3f43e88416113141b0196bdf6c37b444"
SRC_URI[sha256sum] = "15608d7fcf09502d1b8c19b8a63bc22966090ee0761ac9a755e9f747f46d67ab"
PYPI_PACKAGE = "aiortc"
DEPENDS += " \
${PYTHON_PN}-setuptools-scm-native \
${PYTHON_PN}-toml-native \
"
inherit pypi python_setuptools_build_meta
RDEPENDS:${PN} += " \
ffmpeg \
libopus \
libsrtp \
libvpx \
"
BBCLASSEXTEND += "native nativesdk"I did this quick test with the OpenSTLinux distribution that should be released soon. Results may differ against OpenSTLinux ecosystem 3.1
Best regards,
--JM
2022-06-20 7:07 AM
Ok I tried compiling the layer, but received this error:
Could not inherit file classes/python_setuptools_build_meta.bbclass
How do I fix this?
2022-06-20 11:04 PM
Hi @Jaison M
As said, I didn't check with ecosystem-3.1 so I guess this error may be explained so.
For ecosystem-3.1, you could try to remove the DEPENDS variable and replace python_setuptools_build_meta inheritance by setuptools3.
Then, you could also downgrade the aiortc version as the internal build mechanism may not be compatible with ecosystem-3.1 but older versions may be compatible.
Best regards,
--JM
2022-06-21 3:10 PM
Hello sir, like you mentioned in your comment I modified the recipe and tried to compile recipe. This time the it completes compiling, but ends up with one error everytime:
ERROR: python3-aiortc-1.3.2-r0 do_compile: 'python3 setup.py build ' execution failed.
ERROR: python3-aiortc-1.3.2-r0 do_compile: Execution of '/media/jaison/ecrio/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-11-17/build-openstlinuxweston-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/python3-aiortc/1.3.2-r0/temp/run.do_compile.31141' failed with exit code 1:
WARNING: The pip package is not available, falling back to EasyInstall for handling setup_requires/test_requires; this is deprecated and will be removed in a future version.
ERROR: Do not try to fetch `cffi>=1.0.0' for building. Please add its native recipe to DEPENDS.
Traceback (most recent call last):
File "setup.py", line 43, in <module>
setuptools.setup(
File "/media/jaison/ecrio/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-11-17/build-openstlinuxweston-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/python3-aiortc/1.3.2-r0/recipe-sysroot-native/usr/lib/python3.8/site-packages/setuptools/__init__.py", line 143, in setup
_install_setup_requires(attrs)
File "/media/jaison/ecrio/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-11-17/build-openstlinuxweston-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/python3-aiortc/1.3.2-r0/recipe-sysroot-native/usr/lib/python3.8/site-packages/setuptools/__init__.py", line 138, in _install_setup_requires
dist.fetch_build_eggs(dist.setup_requires)
File "/media/jaison/ecrio/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-11-17/build-openstlinuxweston-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/python3-aiortc/1.3.2-r0/recipe-sysroot-native/usr/lib/python3.8/site-packages/setuptools/dist.py", line 718, in fetch_build_eggs
resolved_dists = pkg_resources.working_set.resolve(
File "/media/jaison/ecrio/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-11-17/build-openstlinuxweston-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/python3-aiortc/1.3.2-r0/recipe-sysroot-native/usr/lib/python3.8/site-packages/pkg_resources/__init__.py", line 787, in resolve
raise DistributionNotFound(req, requirers)
pkg_resources.DistributionNotFound: The 'cffi>=1.0.0' distribution was not found and is required by the application
WARNING: exit code 1 from a shell command.I tried adding this to RDEPENDS, even tried with DEPENDS, reduced version numbers ( updated md5 and sha256 variables accordingly ), still no luck. Should I add cffi as a separate layer? I see there is a recipe available at openembedded.org
2022-06-21 10:54 PM
Hi @Jaison M
According to the error, I will try to add python3-cffi-native into the DEPENDS variable.
Best regards,
--JM
2022-06-22 8:02 AM
Thank you sir for the tip, but now a new error pops up,
The last 4 lines of the error log:
/media/jaison/ecrio/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-11-17/build-openstlinuxweston-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/python3-aiortc/1.1.2-r0/build/temp.linux-x86_64-3.8/aiortc.codecs._opus.c:541:10: fatal error: opus/opus.h: No such file or directory
| 541 | #include <opus/opus.h>
| | ^~~~~~~~~~~~~
| compilation terminated.
| error: command 'arm-ostl-linux-gnueabi-gcc' failed with exit status 1
| WARNING: exit code 1 from a shell command.I tried from version 1.3.2 to 1.0.0 so far, will check for version 0.9s now.
I have also uploaded the complete log file from 1.0.0
2022-06-22 10:40 PM
Hi @Jaison M
I guess the libopus library should also be available at compile time hence add it to the DEPENDS variable.
Best regards
--JM
2022-06-23 7:29 AM
Hello sir, like you said I added the libopus to DEPENDS, while compiling I faced similar error for vpx so I also added libvpx to the DEPENDS variable. With that the recipe got compiled successfully.
But when I ad python3-aiortc to the CORE_IMAGE_EXTRA_INSTALL and build st-image-weston image, I'm facing this error now:
ERROR: st-image-weston-1.0-r0 do_rootfs: No manifest generated from: python3-cffi in /media/jaison/ecrio/Distribution-Package/openstlinux-5.10-dunfell-mp1-21-11-17/layers/meta-openembedded/meta-python/recipes-devtools/python/python3-cffi_1.14.0.bb
Also similar error shows up for python3-pycparser at times. How do I fix that? I suppose we are closer to get the aiortc working :smiling_face_with_smiling_eyes:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.