2025-10-28 3:20 PM - edited 2025-10-28 3:22 PM
Hi,
I created a TouchGFX project for the STM32MP135F-DK board. When compiling the project, the error listed below appeared. Despite the error, I was able to load and debug the application on the board using the same procedure applied to any example running on DDR memory.
I verified that "the application binary file 'STM32MP135F-DK.stm32'" was not generated in the folder: Project Folder>\Binary\apps\STM32MP135F-DK.stm32 as per the link:
https://wiki.st.com/stm32mpu/wiki/How_to_install_X-TouchGFX_MPU_Addon
I am using a computer running Windows 11, is it necessary to install any additional software to generate this file?
make -j12 all
arm-none-eabi-size STM32MP135F-DK.elf
text data bss dec hex filename
530448 785264 134112 1449824 161f60 STM32MP135F-DK.elf
Finished building: default.size.stdout
../../Utilities/ImageHeader/postbuild_STM32MP13.sh "C:\ST\STM32CubeIDE_1.18.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344\tools\bin" "STM32MP135F-DK"
Postbuild with Python 3 script
<D> app_name =<>
<D> readelf_path =<C:\ST\STM32CubeIDE_1.18.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344\tools\bin/arm-none-eabi-readelf.exe>
<D> objcopy_path =<C:\ST\STM32CubeIDE_1.18.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344\tools\bin/arm-none-eabi-objcopy.exe>
<D> elf_entry_point =<0xc0000000>
<D> formatted_ep_addr =<c0000000>
Tue Oct 28 17:11:23 2025
Image Name : None
Input file : STM32MP135F-DK_postbuild.bin
Output file : STM32MP135F-DK.stm32
Traceback (most recent call last):
File "C:\TouchGFXProjects\MyApplication_2\Utilities\ImageHeader\Python3\Stm32ImageAddHeader.py", line 243, in <module>
main()
File "C:\TouchGFXProjects\MyApplication_2\Utilities\ImageHeader\Python3\Stm32ImageAddHeader.py", line 233, in main
ret = stm32im.generate(args.image_name, args.input_file, args.output_file)
File "C:\TouchGFXProjects\MyApplication_2\Utilities\ImageHeader\Python3\Stm32ImageAddHeader.py", line 99, in generate
self.image_name = str.encode(image_name) # Output filename is the Image Name
TypeError: descriptor 'encode' for 'str' objects doesn't apply to a 'NoneType' object
postbuild_STM32MP13.sh failed
cp -vf "STM32MP135F-DK.stm32" "../../Binary/apps/STM32MP135F-DK.stm32"
cp: can't stat 'STM32MP135F-DK.stm32': No such file or directory
make[1]: *** [makefile:128: post-build] Error 1
make: *** [makefile:95: all] Error 2
"make -j12 all" terminated with exit code 2. Build might be incomplete.
17:11:23 Build Failed. 2 errors, 0 warnings. (took 4s.224ms)
2025-11-20 4:39 AM
Hello @AMend.7 ,
The scripts in the MPU Add-on require old python 2.7 to be used. Please make sure to have this version used to succeed running the post build steps (hitting 'Run on Target' button in the Designer).
Best Regards,
Akram
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.