2024-11-13 6:50 AM
I created a st-image-qt image using the STM32MP Distribution package and X-LINUX-QT add-on for the STM32MP157F-DK2 board.
I could flash this image using the dd command in Linux and my target board is running correctly.
On the other side, I created a qt quick app using qt 6.7.3(which I could test ok using qt creator) and now I need to add this qt app in my st-image-qt image. I can bitbake this custom recipe doing "bitbake mygui"
I created the custom layer and a custom recipe and added this custom layer to my bblayers. Then, I built the image again with this custom recipe and it worked ok.
The problem is that I'm expecting to find this qt app inside my bin directory, but I can't see it.
SUMMARY = "This is the GUI for Hespect Software medical device"
DESCRIPTION = "Recipe created by bitbake-layers"
LICENSE = "CLOSED"
SECTION = "Mysection"
DEPENDS += " qtbase \
qtdeclarative-native \
qtdeclarative \
qtquick3d \
qtcharts"
RDEPENDS_${PN} += "qtwayland"
EXTRA_OECMAKE += "-DCMAKE_PREFIX_PATH=${STAGING_DIR_HOST}${prefix}"
SRC_URI += "file://main.cpp"
SRC_URI += "file://CMakeLists.txt"
SRC_URI += "file://CMakeLists.txt.user"
SRC_URI += "file://Backendsensors.h"
SRC_URI += "file://Backendsensors.cpp"
SRC_URI += "file://brushfactory.h"
SRC_URI += "file://brushfactory.cpp"
SRC_URI += "file://Main.qml"
# Add SVG images from the assets/images folder
SRC_URI += "file://assets/images/battery-full.svg"
SRC_URI += "file://assets/images/battery-mid.svg"
SRC_URI += "file://assets/images/rss-low.svg"
SRC_URI += "file://assets/images/signal-full.svg"
SRC_URI += "file://assets/images/signal-mid.svg"
SRC_URI += "file://assets/images/battery-low.svg"
SRC_URI += "file://assets/images/rss-full.svg"
SRC_URI += "file://assets/images/rss-mid.svg"
SRC_URI += "file://assets/images/signal-low.svg"
S = "${WORKDIR}/mygui"
do_install () {
install -d ${D}${bindir}
install -m 0775 mygui ${D}${bindir}/
}
FILES_${PN} += "${bindir}/mygui"
inherit cmake_qt5
In my local conf file I added: IMAGE_INSTALL_APPEND += "mygui"
Solved! Go to Solution.
2024-11-16 5:51 PM
The problem was in the syntax. Space at the beginning, and no space at the end works correctly
IMAGE_INSTALL:append = " mygui"
2024-11-14 4:00 AM
yop yop,
u should have a look at:
https://www.blaess.fr/christophe/yocto-lab/sequence-III-1/index.html
its written in french, quite easy language!
look a part :
and from ure side:
IMAGE_INSTALL_APPEND += "mygui"
IMAGE_INSTALL_APPEND += " mygui" (note the space)
hope it helps!
2024-11-16 5:04 AM
I added IMAGE_INSTALL_APPEND += " gui" and compiled the image. When flashing the board I look for /usr/bin/gui but can't find anything. The closes thing I could find is usr/share/examples/gui but it has a "rasterwindow" file, so I think it didn't work
Note: I tried building fresh so I'm using gui instead of mygui
2024-11-16 5:51 PM
The problem was in the syntax. Space at the beginning, and no space at the end works correctly
IMAGE_INSTALL:append = " mygui"
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.