2020-03-30 1:39 AM
hello all
i have a STM32MP157C-EV1, and I want to build an m4 core development and debugging environment in minimal "st-image-core".
M4 firmware created using "STM32CudeIDE" can be debugged in "st-image-weston", but an error occurs in "st-image-core".
What items should be added to "st-image-core.bb" to work normally?
error message :
[ 100.552483] remoteproc remoteproc0: powering up m4
[ 100.555897] remoteproc remoteproc0: Direct firmware load for OpenAMP_TTY_echo_CM4.elf failed with error -2
[ 100.571270] remoteproc remoteproc0: request_firmware failed: -2
[ 100.575829] remoteproc remoteproc0: Boot failed: -2
I will wait for your reply.
Solved! Go to Solution.
2020-04-07 12:23 AM
Hi @Machilus
Good news but anyway still strange behavior.
If you confirm that this "/lib/firmware" is a file issue only happen on custom board and not on EV1, we can suspect the Yocto adaptation you have made to build "st-image-core" for your custom board.
Can you detail further what you have done ?
Thanks
Olivier
2020-04-09 5:56 PM
Hi @OlivierG (ST Employee)
Yes .
This is a phenomenon that only happens on custom board.
I distributed "st-image-core.bb" and dts on custom boards as follows.
<< st-image-core.bb >>
SUMMARY = "OpenSTLinux core image."
LICENSE = "Proprietary"
include recipes-st/images/st-image.inc
inherit core-image
IMAGE_LINGUAS = "en-us"
IMAGE_FEATURES += "\
package-management \
ssh-server-dropbear \
eclipse-debug \
"
#
# INSTALL addons
#
CORE_IMAGE_EXTRA_INSTALL += " \
packagegroup-framework-core-base \
packagegroup-framework-tools-base \
\
${@bb.utils.contains('COMBINED_FEATURES', 'optee', 'packagegroup-optee-core', '', d)} \
${@bb.utils.contains('COMBINED_FEATURES', 'optee', 'packagegroup-optee-test', '', d)} \
${@bb.utils.contains('DISTRO_FEATURES', 'systemd', 'systemd-networkd-configuration', '', d)} \
"
<< Allocate virtual device memory from "dts" >>
reserved-memory {
#address-cells = <1>;
#size-cells = <1>;
ranges;
retram: retram@0x38000000 {
compatible = "shared-dma-pool";
reg = <0x38000000 0x10000>;
no-map;
};
mcuram: mcuram@0x30000000 {
compatible = "shared-dma-pool";
reg = <0x30000000 0x40000>;
no-map;
};
mcuram2: mcuram2@0x10000000 {
compatible = "shared-dma-pool";
reg = <0x10000000 0x40000>;
no-map;
};
vdev0vring0: vdev0vring0@10040000 {
compatible = "shared-dma-pool";
reg = <0x10040000 0x2000>;
no-map;
};
vdev0vring1: vdev0vring1@10042000 {
compatible = "shared-dma-pool";
reg = <0x10042000 0x2000>;
no-map;
};
vdev0buffer: vdev0buffer@10044000 {
compatible = "shared-dma-pool";
reg = <0x10044000 0x4000>;
no-map;
};
};
&m4_rproc {
memory-region = <&retram>, <&mcuram>, <&mcuram2>, <&vdev0vring0>,
<&vdev0vring1>, <&vdev0buffer>;
mboxes = <&ipcc 0>, <&ipcc 1>, <&ipcc 2>;
mbox-names = "vq0", "vq1", "shutdown";
interrupt-parent = <&exti>;
interrupts = <68 1>;
interrupt-names = "wdg";
wakeup-source;
recovery;
status = "okay";
};
After booting up this created distribution,
Error occurs when "OpenAMP_TTY_echo" is built and executed.
This is an error caused by being made into a "/lib/firmware" file.
If you change to a directory, the error disappears.
This is all I did.
Regards.
Machilus.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.