2019-06-16 3:45 PM
I have a generic parallel LCD screen. 24 bits RGB, vsync, hsync, pclk, data_enable, disp_on,..
The examples I see on the wiki only shows the HDMI connection and DSI. How do you configure this for DPI?
Is this a good start? (In the device tree)
panel_backlight: panel-backlight {
compatible = "gpio-backlight";
gpios = <&gpiob 0 GPIO_ACTIVE_HIGH>, <&gpioc 4 GPIO_ACTIVE_HIGH>;
default-on;
status = "okay";
};
lcd0: display@0 {
compatible ="panel-dpi";
label = "lcd";
enable-gpios = <&gpioh 15 GPIO_ACTIVE_HIGH>;
backlight = <&panel_backlight>;
port {
lcd_in: endpoint {
remote-endpoint = <<dc_out_rgb>;
};
};
panel-timing {
clock-frequency = <33000000>;
hactive = <800>;
vactive = <480>;
hfront-porch = <40>;
hback-porch = <40>;
hsync-len = <24>;
vback-porch = <29>;
vfront-porch = <13>;
vsync-len = <3>;
hsync-active = <0>;
vsync-active = <0>;
de-active = <1>;
pixelclk-active = <1>;
};
};and
<dc{
pinctrl-names = "default", "sleep";
pinctrl-0 = <<dc_pins_mx>;
pinctrl-1 = <<dc_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN ltdc */
port {
#address-cells = <1>;
#size-cells = <0>;
ltdc_out_rgb: endpoint {
};
};
/* USER CODE END ltdc */
};
Solved! Go to Solution.
2020-08-04 7:37 AM
Hi
CAN YOU SHARE simple panel ltdc dts configuration, and what drivers you enabled,
i am getting following error
[ 27.659534] [drm:drm_ioctl] pid=799, dev=0xe200, auth=1, DRM_IOCTL_MODE_GETPROPBLOB
[ 27.659547] [drm:drm_mode_object_put.part.0] OBJ ID: 34 (2)
[ 27.769469] [drm:drm_ioctl] pid=799, dev=0xe200, auth=1, DRM_IOCTL_MODE_GETRESOURCES
[ 27.769513] [drm:drm_ioctl] pid=799, dev=0xe200, auth=1, DRM_IOCTL_MODE_GETRESOURCES
[ 27.769550] [drm:drm_ioctl] pid=799, dev=0xe200, auth=1, DRM_IOCTL_MODE_GETCONNECTOR
[ 27.769575] [drm:drm_helper_probe_single_connector_modes] [CONNECTOR:29:DPI-1]
[ 27.769640] [drm:drm_mode_debug_printmodeline] Modeline 35:"800x480" 0 24000 800 1056 1057 1058 480 525 528 529 0x48 0x200000
[ 27.769655] [drm:drm_mode_prune_invalid] Not using 800x480 mode: BAD
[ 27.769678] [drm:drm_mode_object_put.part.0] OBJ ID: 29 (2)
[ 27.769700] [drm:drm_ioctl] pid=799, dev=0xe200, auth=1, DRM_IOCTL_MODE_GETCONNECTOR
[ 27.769724] [drm:drm_mode_object_put.part.0] OBJ ID: 29 (2)
[ 27.770042] [drm:drm_ioctl] pid=799, dev=0xe200, auth=1, DRM_IOCTL_MODE_OBJ_GETPROPERTIES
[ 27.770070] [drm:drm_mode_object_put.part.0] OBJ ID: 29 (2)
[ 27.770094] [drm:drm_ioctl] pid=799, dev=0xe200, auth=1, DRM_IOCTL_MODE_OBJ_GETPROPERTIES
[ 27.770114] [drm:drm_mode_object_put.part.0] OBJ ID: 29 (2)
[ 27.770142] [drm:drm_ioctl] pid=799, dev=0xe200, auth=1, DRM_IOCTL_MODE_GETPROPERTY
[ 27.770161] [drm:drm_ioctl] pid=799, dev=0xe200, auth=1, DRM_IOCTL_MODE_GETPROPERTY
[ 27.770186] [drm:drm_ioctl] pid=799, dev=0xe200, auth=1, DRM_IOCTL_MODE_GETPROPERTY
[ 27.770207] [drm:drm_ioctl] pid=799, dev=0xe200, auth=1, DRM_IOCTL_MODE_GETPROPERTY
[ 27.770238] [drm:drm_ioctl] pid=799, dev=0xe200, auth=1, DRM_IOCTL_MODE_GETPROPERTY
[ 27.770257] [drm:drm_ioctl] pid=799, dev=0xe200, auth=1, DRM_IOCTL_MODE_GETPROPERTY
[ 27.770283] [drm:drm_ioctl] pid=799, dev=0xe200, auth=1, DRM_IOCTL_MODE_GETPROPERTY
[ 27.770301] [drm:drm_ioctl] pid=799, dev=0xe200, auth=1, DRM_IOCTL_MODE_GETPROPERTY
[ 27.770323] [drm:drm_ioctl] pid=799, dev=0xe200, auth=1, DRM_IOCTL_MODE_GETPROPERTY
[ 27.770342] [drm:drm_ioctl] pid=799, dev=0xe200, auth=1, DRM_IOCTL_MODE_GETPROPERTY
[ 27.770387] [drm:drm_ioctl] pid=799, dev=0xe200, auth=1, DRM_IOCTL_MODE_GETENCODER
[ 27.770402] [drm:drm_ioctl] pid=799, ret = -2
[ 34.320078] random: crng init done
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.