2024-08-15 3:34 AM - edited 2024-08-15 3:42 AM
I want to test the memory by using U-boot.
I'm reading the DDR memory from 0xC0000000 to 0xE0000000 with the pattern 0xFFFFFFF. But I don't have premision to read the memory. How can I solve this issue?
STM32MP> mtest 0xC0000000 0xE0000000 0xFFFFFFFF
Testing c0000000 ... e0000000:
Iteration: 1
Pattern FFFFFFFF Writing... Reading...Iteration: 2
Pattern 00000001 Writing... E/TC:0 tzc_it_handler:79 TZC permission failure
E/TC:0 dump_fail_filter:420 Permission violation on filter 0
E/TC:0 dump_fail_filter:425 Violation @0xf8803000, non-secure privileged read, AXI ID 4a0
E/TC:0 tzc_it_handler:79 TZC permission failure
E/TC:0 dump_fail_filter:420 Permission violation on filter 0
E/TC:0 dump_fail_filter:425 Violation @0xf8804000, non-secure privileged read, AXI ID 4a0
My U-boot Device Tree for the memory.
memory@c0000000 {
device_type = "memory";
reg = <0xc0000000 0x20000000>;
/* USER CODE BEGIN memory */
/* USER CODE END memory */
};
reserved-memory {
#address-cells = <1>;
#size-cells = <1>;
ranges;
/* USER CODE BEGIN reserved-memory */
optee@de000000 {
reg = <0xde000000 0x2000000>;
no-map;
};
mcuram2:mcuram2@10000000{
compatible = "shared-dma-pool";
reg = <0x10000000 0x40000>;
no-map;
};
vdev0vring0:vdev0vring0@10040000{
compatible = "shared-dma-pool";
reg = <0x10040000 0x1000>;
no-map;
};
vdev0vring1:vdev0vring1@10041000{
compatible = "shared-dma-pool";
reg = <0x10041000 0x1000>;
no-map;
};
vdev0buffer:vdev0buffer@10042000{
compatible = "shared-dma-pool";
reg = <0x10042000 0x4000>;
no-map;
};
mcu_rsc_table:mcu-rsc-table@10048000{
compatible = "shared-dma-pool";
reg = <0x10048000 0x8000>;
no-map;
};
mcuram:mcuram@30000000{
compatible = "shared-dma-pool";
reg = <0x30000000 0x40000>;
no-map;
};
retram:retram@38000000{
compatible = "shared-dma-pool";
reg = <0x38000000 0x10000>;
no-map;
};
/* USER CODE END reserved-memory */
};
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.