2022-06-15 7:43 AM
Hi, I am looking all through the wiki, but I do not see any clue on using the tampers as a wakeup source.
How can I configure the tampers to wake up the stm32mp1 from low power modes?
Is it posible to wake up from VBAT? Or is VBAT only a energy mode to maintain the data in the memories? Can I run a piece of code in VBAT mode? If so, how could I do it? What restrictions do apply?
When I say a piece of code, I mean it can be baremetal or linux or whatever it can run.
Best regards,
Andrés
Solved! Go to Solution.
2022-06-27 8:18 AM
Hi AGamb.4 (Community Member)
There is the procedure in the wiki here linux side.
https://wiki.st.com/stm32mpu/wiki/TAMP_device_tree_configuration
VBAT presence allows to have the backup domain powered when VDD is not present (as in STM32 MCUs). But CPUs are not powered. Refer to the product reference manual for more details.
Regards,
Olivier
2022-06-27 8:18 AM
Hi AGamb.4 (Community Member)
There is the procedure in the wiki here linux side.
https://wiki.st.com/stm32mpu/wiki/TAMP_device_tree_configuration
VBAT presence allows to have the backup domain powered when VDD is not present (as in STM32 MCUs). But CPUs are not powered. Refer to the product reference manual for more details.
Regards,
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.