2021-02-19 6:54 AM
Hello everybody,
i have a problem booting the SD card. The problem occurred after I copied the device tree (.dtb) from my project from STM32CubeMx to the STM32MP157A under / boot. When booting, the U-Boot and the start kernel run endlessly. How can I solve the problem?
Thanks a lot
Here is the output from the board:
U-Boot 2018.11-stm32mp-r2 (Nov 14 2018 - 16:10:06 +0000)
CPU: STM32MP157AAC Rev.B
Model: STMicroelectronics STM32MP157A-DK1 Discovery Board
Board: stm32mp1 in trusted mode (st,stm32mp157a-dk1)
Board: MB1272 Var1 Rev.C-01
Watchdog enabled
DRAM: 512 MiB
Clocks:
- MPU : 650 MHz
- MCU : 208.878 MHz
- AXI : 266.500 MHz
- PER : 24 MHz
- DDR : 533 MHz
*******************************************
* WARNING 500mA power supply detected *
* Current too low, use a 3A power supply! *
*******************************************
NAND: 0 MiB
MMC: STM32 SDMMC2: 0
In: serial
Out: serial
Err: serial
Net: eth0: ethernet@5800a000
Boot over mmc0!
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:4...
Found U-Boot script /boot.scr.uimg
1553 bytes read in 1 ms (1.5 MiB/s)
## Executing script at c4100000
Scanning mmc 0:4...
Found /mmc0_stm32mp157a-dk1_extlinux/extlinux.conf
Retrieving file: /mmc0_stm32mp157a-dk1_extlinux/extlinux.conf
237 bytes read in 1 ms (231.4 KiB/s)
Retrieving file: /mmc0_stm32mp157a-dk1_extlinux/../splash.bmp
46180 bytes read in 3 ms (14.7 MiB/s)
1: stm32mp157a-dk1-sdcard
Enter choice: 1: stm32mp157a-dk1-sdcard
Retrieving file: /uImage
6569168 bytes read in 291 ms (21.5 MiB/s)
append: root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200
Retrieving file: /stm32mp157a-dk1.dtb
103076 bytes read in 6 ms (16.4 MiB/s)
## Booting kernel from Legacy Image at c2000000 ...
Image Name: Linux-4.19.9
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 6569104 Bytes = 6.3 MiB
Load Address: c2000040
Entry Point: c2000040
Verifying Checksum ... OK
## Flattened Device Tree blob at c4000000
Booting using the fdt blob at 0xc4000000
XIP Kernel Image ... OK
Using Device Tree in place at c4000000, end c401c2a3
Starting kernel ...
NOTICE: CPU: STM32MP157AAC Rev.B
NOTICE: Model: STMicroelectronics STM32MP157A-DK1 Discovery Board
NOTICE: Board: MB1272 Var1 Rev.C-01
INFO: Reset reason (0x214):
INFO: IWDG2 Reset (rst_iwdg2)
INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
INFO: Product_below_2v5=1: HSLVEN update is
INFO: destructive, no update as VDD>2.7V
NOTICE: BL2: v2.0(debug):
NOTICE: BL2: Built : 13:13:37, Oct 2 2018
INFO: BL2: Doing platform setup
INFO: PMIC version = 0x10
INFO: RAM: DDR3-1066/888 bin G 1x4Gb 533MHz v1.41
INFO: Memory size = 0x20000000 (512 MB)
INFO: BL2 runs SP_MIN setup
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x2fff0000
INFO: Image id=4 loaded: 0x2fff0000 - 0x30000000
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0100000
INFO: STM32 Image size : 746647
WARNING: Skip signature check (header option)
INFO: Image id=5 loaded: 0xc0100000 - 0xc01b6497
INFO: read version 0 current version 0
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0x2fff0000
INFO: SPSR = 0x1d3
INFO: PMIC version = 0x10
NOTICE: SP_MIN: v2.0(debug):
NOTICE: SP_MIN: Built : 13:13:37, Oct 2 2018
INFO: ARM GICv2 driver initialized
INFO: stm32mp HSI (18): Secure only
INFO: stm32mp HSE (20): Secure only
INFO: stm32mp PLL2 (27): Secure only
INFO: stm32mp PLL2_R (30): Secure only
INFO: SP_MIN: Initializing runtime services
INFO: SP_MIN: Preparing exit to normal world
U-Boot 2018.11-stm32mp-r2 (Nov 14 2018 - 16:10:06 +0000)
CPU: STM32MP157AAC Rev.B
Model: STMicroelectronics STM32MP157A-DK1 Discovery Board
Board: stm32mp1 in trusted mode (st,stm32mp157a-dk1)
Board: MB1272 Var1 Rev.C-01
Watchdog enabled
DRAM: 512 MiB
Clocks:
- MPU : 650 MHz
- MCU : 208.878 MHz
- AXI : 266.500 MHz
- PER : 24 MHz
- DDR : 533 MHz
*******************************************
* WARNING 500mA power supply detected *
* Current too low, use a 3A power supply! *
*******************************************
NAND: 0 MiB
MMC: STM32 SDMMC2: 0
In: serial
Out: serial
Err: serial
Net: eth0: ethernet@5800a000
Boot over mmc0!
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:4...
Found U-Boot script /boot.scr.uimg
1553 bytes read in 1 ms (1.5 MiB/s)
## Executing script at c4100000
Scanning mmc 0:4...
Found /mmc0_stm32mp157a-dk1_extlinux/extlinux.conf
Retrieving file: /mmc0_stm32mp157a-dk1_extlinux/extlinux.conf
237 bytes read in 1 ms (231.4 KiB/s)
Retrieving file: /mmc0_stm32mp157a-dk1_extlinux/../splash.bmp
46180 bytes read in 3 ms (14.7 MiB/s)
1: stm32mp157a-dk1-sdcard
Enter choice: 1: stm32mp157a-dk1-sdcard
Retrieving file: /uImage
6569168 bytes read in 291 ms (21.5 MiB/s)
append: root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200
Retrieving file: /stm32mp157a-dk1.dtb
103076 bytes read in 6 ms (16.4 MiB/s)
## Booting kernel from Legacy Image at c2000000 ...
Image Name: Linux-4.19.9
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 6569104 Bytes = 6.3 MiB
Load Address: c2000040
Entry Point: c2000040
Verifying Checksum ... OK
## Flattened Device Tree blob at c4000000
Booting using the fdt blob at 0xc4000000
XIP Kernel Image ... OK
Using Device Tree in place at c4000000, end c401c2a3
Starting kernel ...
2021-03-17 1:20 AM
Hello,
I suggest to use the wiki https://wiki.st.com/stm32mpu/wiki/Main_Page
The Getting started for DK2 will help you to reflash your board https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2
(The tutorial is for DK2, but very same for dk1, except you need to select the dk1 flashlayout)
Note that SD-Card could also be populated directly on Unix (e.g. with an USB => SD-Card adapter)
https://wiki.st.com/stm32mpu/wiki/How_to_populate_the_SD_card_with_dd_command
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.