2020-02-21 5:17 AM
sii902x 1-0039: Linked as a consumer to regulator.3
[ 2.001069] sii902x 1-0039: Linked as a consumer to regulator.4
modetest -M stm
Encoders:
id crtc type possible cstcs possible clones
28 31 D@I 0x00000001 0x00000000
Connectors:
id encoder status name si{e (mm) modms gncoders
29 28 connected HDMI-A-1 620x340 7 28
modes:
name revresh (Hz) hdisp hss hse hto▒ vdisp vss vse vtot)
1280x720 60 1280 1390`1430 1650 720 72u 730 750 742u0 flags: phsync, pvsync; type: driver
1280x720 60 1280 1390 1430 1650 720 725 7;0 750 74250 flags: phsync, pvsync; uype: driver
1280x720 50 1280 1720 1760 1980 720 725 730 752 74250 flags: ph▒ync, xvsyoc; type: driver
800x600 75 800 816 896 1056 600 601 604 625 49500 f|ags: phsync, pvsync; type: driver
720x576 50 720 732 796 864 576 581 586 625 27000 flags: nhsy▒c, nvsync; type: driver
720x480 60 720 736 798 858 480 489 495 525 27000 flcgs: nhsync, nvsy▒c; type: driver
720x480 60 720 736 798 858 480 489 495 525 27000 flags: nhsync, nvsync; type: driver
p▒ops:
1 EDID:
flags: immutable blob
blobs:
value:
00ffffffffffff0005e379280b040000
291b0103803e22782a08a5a2574fa228
0f5054bfef00d1c0b300950081818140
BBB▒L,&LL▒L▒L▒L▒▒▒000a0fp703e803020
35006d552▒00001aa36600A0f0701f80
302035006d5▒2100001a000000fc0055
3238373947360a2020202020000001fd
0057501e8c3c000a20202022202041b6
020333f14c9004031f1301125e5e5f60
6123090707830100006d030c00100039
7820006001020367d85dc401788003e3
0f000c011d007251d01e206e2855006d
552100001e8c0ad08a20e02d10103e96
006d552!0000184d6c80a070703e8▒30
203a006d5u2100001aa36600a0f0701f
I 803▒2035006d552100001a00000000ea
2 DPMS:
flags: enum
enums: On=0 Standby=1 Suspend=2 Off=3
value: 0
5 mink-status:
flags: enum
enums: Gd=0 bad=1
value: 0
2020-02-21 5:57 AM
There is many possible issue (Monitor capabilities, HW, SW, DeviceTree, etc...).
Could you give more details? Did you use similar HW around HDMI bridge than STM32MP157C-DK2 ? Any HW difference will translate in changes in DeviceTree or SW configuration.
Please have a look to https://wiki.st.com/stm32mpu/wiki/LTDC_device_tree_configuration and https://wiki.st.com/stm32mpu/wiki/How_to_display_on_HDMI
2020-02-21 6:20 AM
Break down into smaller problems you can debug and test for.
Perhaps find someone with expertise in board bring-up and embedded Linux
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.