2023-06-09 2:41 PM
I was trying to use the GPIO expension connector on the STM32MP15 Discovery Kit MB1272 and the clock wasn't working on SPI5. When I checked the CubeMX configuration against the schematic for the discovery kit, I leaned that the clock signal is going to the Arduino connector instead of the GPIO expansion. The schematic insinuates that PF7 is SPI5_SCK, when it is actually PH6. Is this a known issue?
Solved! Go to Solution.
2023-06-12 5:45 AM
HI @Aaron Lebahn
From STM32MP157 datasheet, SPI5_SCK is available on either PF7-AF5, PH6-AF5 or PK0-AF5.
So, Schematics is OK in using PF7 for SPI5_SCK.
In Default Device tree (e.g. Starter Package), SPI5_SCK is defined on PF7.
Maybe a Device tree pinmux issue or overlook on your side.
Regards.
2023-06-12 5:45 AM
HI @Aaron Lebahn
From STM32MP157 datasheet, SPI5_SCK is available on either PF7-AF5, PH6-AF5 or PK0-AF5.
So, Schematics is OK in using PF7 for SPI5_SCK.
In Default Device tree (e.g. Starter Package), SPI5_SCK is defined on PF7.
Maybe a Device tree pinmux issue or overlook on your side.
Regards.
2023-06-12 12:38 PM
Hi @PatrickF
Thanks for your reply. I was able to modify the setting in STM32CubeMX to set SPI5_SCK to PF7. I tried to do that before but didn't realize it wouldn't show as an option until I disabled the existing setting for SPI5_SCK. After setting the mux correctly, I'm seeing the clock signal on the GPIO expansion as expected.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.