2023-07-20 4:18 AM - edited 2023-07-20 4:54 AM
I am working on yocto project. I started with a custom board based on stm32mp157. You can find the board description in this link custom board. Vendor has a board support package in dunfell version. But I am doing my project in kirkstone version. I have choosen my distribution packgae from the openstlinuxdistribution. I have following build configuration for creating the image:
Build Configuration: BB_VERSION = "2.0.0" BUILD_SYS = "x86_64-linux" NATIVELSBSTRING = "universal" TARGET_SYS = "arm-emt_eglfs-linux-gnueabi" MACHINE = "emsbc-argon" DISTRO = "emt-eglfs" DISTRO_VERSION = "1.3" TUNE_FEATURES = "arm vfp cortexa7 neon vfpv4 thumb callconvention-hard" TARGET_FPU = "hard" DISTRO_CODENAME = "kirkstone" ACCEPT_EULA_emsbc-argon = "1" GCCVERSION = "11.%" PREFERRED_PROVIDER_virtual/kernel = "linux-stm32mp-argon" meta-emtrion-emsbc-argon meta-emtrion = "<unknown>:<unknown>" meta = "HEAD:f7766da462905ec67bf549d46b8017be36cd5b2a" meta-oe meta-initramfs meta-multimedia meta-python meta-networking meta-webserver meta-filesystems meta-perl = "HEAD:05dcac98473402d87e0af73bbc2c5a6a840abe93" meta-qt5 = "HEAD:5b71df60e523423b9df6793de9387f87a149ac42" meta-st-stm32mp = "HEAD:ca501bd7dbe023682903ceedddaacd940b0898f4" meta-st-openstlinux = "HEAD:cb736b403d0fef2a02390695613b6b4bb13ca1b7" meta-gnome = "HEAD:05dcac98473402d87e0af73bbc2c5a6a840abe93"
I have created two custom layer, which added in the bblayers.conf file. I have the following error:
Summary: 1 task failed: virtual:nativesdk:/home/hico/work/emtrion/argon-yocto/test-st-yocto/layers/openembedded- core/meta/recipes-core/glibc/glibc-locale_2.35.bb:do_package
You can find the log file in this link logfile. Does anyone have any idea to solve this error?
2023-08-03 6:11 AM
Hello @ahamod3.1416 ,
Are you still stuck with this issue ?
I cannot access to your logfile that will be mandatory to check the error. Can you put it in attachment please ?
Kind regards,
Erwan.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.