STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

u-boot splash change problem

Hi all ~I'm using our custom board with STM32MP157c MPU. I'm almost done with everything, and finally I'm going to change the u-boot and kernel splash images.I referred to the link for changing the u-boot splash image and I think it's very simple.htt...

Resolved! Uploading flash layout changes with Tf-a 2.6.

Hello,we (me and @Daniel Laszlo Sitzer​ ) and are working with a product based on the STM32MP157A and using TF-A, U-Boot (but not OPTEE).We are in the process for transitioning from TF-A v2.4 to v2.6 and are tryingto understand how we are supposed to...

d3 by Associate
  • 2333 Views
  • 1 replies
  • 0 kudos

Is it possible to connect a camera module to STM32MP157D-DK1 discovery kit? if so how and what camera module ?

Please can you specify camera module for my application and please suggest any camera module that i can use according to the below mentioned camera specifications1)Camera should be of 5MP/2MP.2)Camera interface should be of DCMI protocol.3)Camera sho...

SM.22 by Associate II
  • 5807 Views
  • 8 replies
  • 0 kudos

Resolved! Problem booting from eMMC on Rev.Z

I have a strange problem booting from eMMC (Kingstone EMMC04G-M627-X03U) on STM32MP153CAA Rev.Z.By boot failure I mean fallback to serial boot (DFU over USB). Situation is as follows:Cold start never fails (Power-on Reset).Reset pin (Pad Reset from N...

"pip3 install ***" error

hi st expertWhen i use pip3 install some package on board, i get some error as follew:running build_extbuilding '_cffi_backend' extensioncreating build/temp.linux-armv7l-3.8creating build/temp.linux-armv7l-3.8/c           arm-ostl-linux-gnueabi-gcc ...

ttao.1 by Associate II
  • 3966 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.