2019-09-08 11:54 PM
I tried booting via TFTP boot and got the following reply
BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3
DHCP client bound to address 192.168.1.2 (766 ms)
missing environment variable: pxeuuid
missing environment variable: bootfile
Retrieving file: pxelinux.cfg/01-00-80-e1-42-56-51
Using ethernet@5800a000 device
TFTP from server 192.168.1.94; our IP address is 192.168.1.2
Filename 'pxelinux.cfg/01-00-80-e1-42-56-51'.
Load address: 0xc4200000
Loading: #
0 Bytes/s
done
Bytes transferred = 248 (f8 hex)
Config file found
Select the boot mode
1: Linux 4.19.9
Enter choice: 1: Linux 4.19.9
missing environment variable: bootfile
Retrieving file: uImage
Using ethernet@5800a000 device
TFTP from server 192.168.1.94; our IP address is 192.168.1.2
'.lename 'uImage
Load address: 0xc2000000
Loading: *
TFTP error: 'File not found' (1)
Not retrying...
for failure retrieving kernel
this is my /tftpboot tree
.
├── pxelinux.cfg
│ ├── 01-00-80-e1-42-56-51 -> default-arm-stm32mp
│ └── default-arm-stm32mp
├── stm32mp157c-dk2.dtb
└── uImage
I tested the TFTP server is available, all files are available for download.
Where is the problem?
Solved! Go to Solution.
2019-09-09 6:09 PM
The reason is default-arm-stm32mp file use CRLF not LF,now it work
2019-09-09 1:04 AM
Hi @Jzhua
Can you please confirm you have followed this guideline
https://wiki.st.com/stm32mpu/wiki/How_to_boot_the_kernel_via_TFTP_from_U-Boot
Thx
Olivier
2019-09-09 1:32 AM
yes,I was followed this guideline
2019-09-09 7:57 AM
Hi @Jzhua
I succeed to boot on tftp with the procedure.
content of my tftpboot directory ( I used artifact from defaut st-image-weston stm32mp1-disco image)
/tftboot :
drwxrwxr-x 2 osboxes osboxes 4096 Sep 9 12:44 pxelinux.cfg
-rwxrwxrwx 1 osboxes osboxes 69510 Sep 9 10:31 stm32mp157c-dk2--4.19-r0-stm32mp1-disco-20190909122915.dtb
lrwxrwxrwx 1 osboxes osboxes 68 Sep 9 12:31 stm32mp157c-dk2.dtb -> /tftpboot/stm32mp157c-dk2--4.19-r0-stm32mp1-disco-20190909122915.dtb
lrwxrwxrwx 1 osboxes osboxes 59 Sep 9 12:30 uImage -> /tftpboot/uImage--4.19-r0-stm32mp1-disco-20190909122915.bin
-rwxrw-rw- 1 osboxes osboxes 6555552 Sep 9 10:29 uImage--4.19-r0-stm32mp1-disco-20190909122915.bin
Content of pxelinux.cfg/01-00-80-e1-42-4c-e8
menu title Select the boot mode
DEFAULT ramfs
LABEL ramfs
KERNEL uImage
FDT stm32mp157c-dk2.dtb
APPEND rootwait rw earlyprintk console=ttyS3,115200
I need to remove line 'INITRD uInitrd' in order it works.
Problem looks to come from this broken line in your trace :
TFTP from server 192.168.1.94; our IP address is 192.168.1.2
'.lename 'uImage
On my side I got :
TFTP from server 10.xx.***.49; our IP address is 10.xx.***.120
Filename 'uImage'.
Check for any syntax issue ?
Hope it help
Olivier
2019-09-09 6:09 PM
The reason is default-arm-stm32mp file use CRLF not LF,now it work
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.