2026-02-10 12:45 PM
I've got a custom board with an STM32MP135AAE3 talking to an eMMC (THGBMTG5D1LBAIL if it makes a difference). I've discovered that if I write from SYSTEM to the eMMC using DMA (HAL_MMC_WriteBlocks_DMA) it works fine, but if I use anything in RAM (SRAM1, SRAM2, or SRAM3) as the source, the DMA fails immediately.
If it helps, the SDMMC2 registers inside SDMMC2_IRQHandler() are: STA=0x8001010; DCOUNT=0x200; DCTRL=0x90; IDMACTRL=0x1; MASK=0x11A
Is this a known limitation of the IDMA? If not, is it something I'm somehow initializing incorrectly?
Solved! Go to Solution.
2026-02-11 7:50 AM
Hi,
I think this the root cause as FSBL loaded by BootROM is limited to 128KB on STM32MP13
https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_code_overview#On_STM32MP1-lines_4
Regards.
2026-02-10 11:31 PM
Hi @cbcooper
Maybe check that ETZPC configuration for SDMMC2, SYSRAM and SRAMx are consistent.
Check that the right SRAMs addresses are used for SDMMC DMA.
Regards.
2026-02-11 7:38 AM
I think you're right about the ETZPC configuration (this is the first time I've programmed an STM32 chip where I had to think about secure vs. non-secure memory). All I had was this line:
LL_ETZPC_SetSecureSysRamSize(ETZPC, 0);but if I add these 3 lines;
HAL_ETZPC_Set_SRAM1_PeriphProtection(ETZPC, LL_ETZPC_PERIPH_PROTECTION_READ_WRITE_NONSECURE);
HAL_ETZPC_Set_SRAM2_PeriphProtection(ETZPC, LL_ETZPC_PERIPH_PROTECTION_READ_WRITE_NONSECURE);
HAL_ETZPC_Set_SRAM3_PeriphProtection(ETZPC, LL_ETZPC_PERIPH_PROTECTION_READ_WRITE_NONSECURE);then STM32_Programmer_CLI.exe hangs when trying to download the application.
Why would the download hang? I assumed STM32_Programmer_CLI. would download the application first and succeed at that, and then run the program (which could fail/crash/hang if those lines are wrong) but how can adding those lines affect the download?
2026-02-11 7:45 AM
Is the BootROM only able to upload into SYSRAM (and not SRAM1/SRAM2/SRAM3)? Adding those 3 lines increased the payload size from 0x1F57C = 128,380 bytes to 0x20588 = 132,488 bytes. I have a check in my LD file:
ASSERT(. <= ORIGIN(RAM) + LENGTH(RAM), "RAM overflow: sections exceed available RAM")where
MEMORY {
SYSRAM_BASE (rwx) : ORIGIN = 0x2FFE0000, LENGTH = 128K
SRAM1_BASE (rwx) : ORIGIN = 0x30000000, LENGTH = 16K
SRAM2_BASE (rwx) : ORIGIN = 0x30004000, LENGTH = 8K
SRAM3_BASE (rwx) : ORIGIN = 0x30006000, LENGTH = 8K
/* InternalMEM = SYSRAM + SRAM1 + SRAM2 + SRAM3 */
InternalMEM (rwx) : ORIGIN = 0x2FFE0000, LENGTH = 160K
DDR_BASE (rwx) : ORIGIN = 0xC0000000, LENGTH = 128M
}
/* Select Memory in which code has to be placed and offset of code from start of this memory */
REGION_ALIAS("RAM", InternalMEM);but do I instead need to check
ASSERT(. <= ORIGIN(SYSRAM_BASE) + LENGTH(SYSRAM_BASE), "RAM overflow: sections exceed available RAM")
2026-02-11 7:50 AM
Hi,
I think this the root cause as FSBL loaded by BootROM is limited to 128KB on STM32MP13
https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_code_overview#On_STM32MP1-lines_4
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.