2025-06-11 1:37 AM
We have a custom design based on STMP32MP133A na an spi NAND. On paper, using the u-boot diagnostic commands, everything is working correctly.
NOTICE: CPU: STM32MP133A Rev.Y
NOTICE: Model: Zehnder CCPRO A1R Board
INFO: PMIC version = 0x21
INFO: Reset reason (0x35):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe0000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.6-stm32mp1-r2.1(debug):v2.6-dirty(a1f02f4f)
NOTICE: BL2: Built : 13:14:26, Nov 23 2021
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-1066 bin F 1x2Gb 533MHz v1.53
INFO: Memory size = 0x10000000 (256 MB)
INFO: DFU USB START...
INFO: handle USB : Suspend int
INFO: USB Suspend mode
INFO: handle USB : Reset
INFO: handle USB : Reset
INFO: phase ID :3, Manifestation 0 at c716d456
INFO: Receive DFU Detach
INFO: DFU USB STOP...
INFO: BL2: Loading image id 1
INFO: Loading image id=1 at address 0x30006000
INFO: Image id=1 loaded: 0x30006000 - 0x30006246
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x30006000
INFO: FCONF: Reading firmware configuration information for: mce_config
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0xce000000
INFO: Image id=4 loaded: 0xce000000 - 0xce00001c
INFO: OPTEE ep=0xce000000
INFO: OPTEE header info:
INFO: magic=0x4554504f
INFO: version=0x2
INFO: arch=0x0
INFO: flags=0x0
INFO: nb_images=0x1
INFO: BL2: Loading image id 8
INFO: Loading image id=8 at address 0xce200000
INFO: Image id=8 loaded: 0xce200000 - 0xce277260
INFO: BL2: Loading image id 2
INFO: Loading image id=2 at address 0xc0400000
INFO: Image id=2 loaded: 0xc0400000 - 0xc040d740
INFO: BL2: Skip loading image id 16
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0000000
INFO: Image id=5 loaded: 0xc0000000 - 0xc00e872c
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0xce200000
INFO: SPSR = 0x1d3
I/TC: Early console on UART#4
I/TC:
I/TC: Non-secure external DT found
I/TC: Embedded DTB found
I/TC: OP-TEE version: 3.16.0-6-gbe2b808b6-dev (gcc version 11.5.0 (GCC)) #7 Mon Jun 9 12:47:36 PM UTC 2025 arm
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: WARNING: All debug access are allowed
E/TC:0 0 stm32mp1_cpu_opp_is_supported:210 Invalid opp-supported-hw 0x2
E/TC:0 0 stm32mp1_cpu_opp_is_supported:210 Invalid opp-supported-hw 0x2
E/TC:0 0 stm32mp1_cpu_opp_is_supported:210 Invalid opp-supported-hw 0x2
E/TC:0 0 stm32mp1_cpu_opp_is_supported:210 Invalid opp-supported-hw 0x2
E/TC:0 0 probe_driver_node:402 Failed to probe stm32mp1-cpu-opp on node cpu0-opp-table: 0xffff0000
E/TC:0 0 print_probe_list:358 |- Driver stm32mp1-cpu-opp on node cpu0-opp-table failed
I/TC: Platform stm32mp1: flavor PLATFORM_FLAVOR - DT stm32mp133a-ccproa1r.dts
I/TC: DTB enables console (non-secure)
E/TC:0 0 call_initcalls:43 Initcall __text_start + 0x0006f080 failed
E/TC:0 0 probe_dt_drivers:739 Probe sequence result: 0
E/TC:0 0 print_probe_list:358 |- Driver stm32mp1-cpu-opp on node cpu0-opp-table failed
E/TC:0 0 regulator_get_by_regulator_name:95 vdd_adc not found
E/TC:0 0 scmi_regulator_consumer_init:295 regulator vdd_adc not found, skipped
I/TC: Primary CPU switching to normal world boot
optee optee: OP-TEE: revision 3.16 (be2b808b)
U-Boot 2021.10-stm32mp-r2.1 (Jun 11 2025 - 08:13:23 +0000)
CPU: STM32MP133A Rev.Y
Model: Zehnder CCPRO A1R Board
Board: stm32mp1 in trusted mode (st,stm32mp133a-ccproa1r)
DRAM: 256 MiB
optee optee: OP-TEE: revision 3.16 (be2b808b)
Clocks:
- MPU : 650 MHz
- AXI : 266.500 MHz
- PER : 24 MHz
- DDR : 533 MHz
WDT: Started with servicing (32s timeout)
NAND: 0 MiB
MMC:
Loading Environment from nowhere... OK
In: serial
Out: serial
Err: serial
invalid MAC address 0 in OTP 00:00:00:00:00:00
Net: No ethernet found.
Hit any key to stop autoboot: 0
Boot over usb0!
DFU alt info setting: done
#
FlashLayout received, size = 552
DOWNLOAD ... OK
Ctrl+C to exit ...
spi-nand: spi_nand mt29f4g01abafdwb@0: Micron SPI NAND was found.
spi-nand: spi_nand mt29f4g01abafdwb@0: 512 MiB, block size: 256 KiB, page size: 4096, OOB size: 256
DFU alt info setting: using id 'spi-nand0,0'
using id 'spi-nand0,1'
using id 'spi-nand0,2'
using id 'spi-nand0,3'
done
crq->brequest:0x0
#dfu-utils says:
Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2016 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to http://sourceforge.net/p/dfu-util/tickets/
Opening DFU capable USB device...
ID 0483:df11
Run-time device DFU version 0110
Claiming USB DFU Interface...
Setting Alternate Setting #3 ...
dfu-util: Cannot set alternate interface
74 angelo@angelo-Precision-7550:~/DEV/yocto-zehnder$
74 angelo@angelo-Precision-7550:~/DEV/yocto-zehnder$ sh program.sh[A
sh: 0: cannot open program.sh[A: No such file
2 angelo@angelo-Precision-7550:~/DEV/yocto-zehnder$ sh program.sh
+ dfu-util -a 0 -D build/tmp-glibc/deploy/images/ccproa1r/arm-trusted-firmware/tf-a-stm32mp133a-ccproa1r-usb.stm32
dfu-util 0.9
Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2016 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to http://sourceforge.net/p/dfu-util/tickets/
dfu-util: Invalid DFU suffix signature
dfu-util: A valid DFU suffix will be required in a future dfu-util release!!!
Opening DFU capable USB device...
ID 0483:df11
Run-time device DFU version 0110
Claiming USB DFU Interface...
Setting Alternate Setting #0 ...
Determining device status: state = dfuIDLE, status = 0
dfuIDLE, continuing
DFU mode device DFU version 0110
Device returned transfer size 1024
Copying data from PC to DFU device
Download [=========================] 100% 92948 bytes
Download done.
state(7) = dfuMANIFEST, status(0) = No error condition is present
state(2) = dfuIDLE, status(0) = No error condition is present
Done!
+ dfu-util -a 0 -e
dfu-util 0.9
Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2016 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to http://sourceforge.net/p/dfu-util/tickets/
Opening DFU capable USB device...
ID 0483:df11
Run-time device DFU version 0110
Claiming USB DFU Interface...
Setting Alternate Setting #0 ...
Determining device status: state = dfuIDLE, status = 0
dfuIDLE, continuing
DFU mode device DFU version 0110
Device returned transfer size 1024
+ sleep 2
+ dfu-util -a 0 -D build/tmp-glibc/deploy/images/ccproa1r/fip/fip-stm32mp133a-ccproa1r-optee.img
dfu-util 0.9
Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2016 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to http://sourceforge.net/p/dfu-util/tickets/
dfu-util: Invalid DFU suffix signature
dfu-util: A valid DFU suffix will be required in a future dfu-util release!!!
Opening DFU capable USB device...
ID 0483:df11
Run-time device DFU version 0110
Claiming USB DFU Interface...
Setting Alternate Setting #0 ...
Determining device status: state = dfuIDLE, status = 0
dfuIDLE, continuing
DFU mode device DFU version 0110
Device returned transfer size 1024
Copying data from PC to DFU device
Download [=========================] 100% 1496150 bytes
Download done.
state(7) = dfuMANIFEST, status(0) = No error condition is present
state(2) = dfuIDLE, status(0) = No error condition is present
Done!
+ dfu-util -a 0 -e
dfu-util 0.9
Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2016 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to http://sourceforge.net/p/dfu-util/tickets/
Opening DFU capable USB device...
ID 0483:df11
Run-time device DFU version 0110
Claiming USB DFU Interface...
Setting Alternate Setting #0 ...
Determining device status: state = dfuIDLE, status = 0
dfuIDLE, continuing
DFU mode device DFU version 0110
Device returned transfer size 1024
+ sleep 10
+ dfu-util -a 0 -D build/tmp-glibc/deploy/images/ccproa1r/flashlayout_ccproa1r-hwv-image-eng/optee/FlashLayout_spinand-2-128_stm32mp133a-ccproa1r-optee.tsv
dfu-util 0.9
Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2016 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to http://sourceforge.net/p/dfu-util/tickets/
dfu-util: Invalid DFU suffix signature
dfu-util: A valid DFU suffix will be required in a future dfu-util release!!!
Opening DFU capable USB device...
ID 0483:df11
Run-time device DFU version 0110
Claiming USB DFU Interface...
Setting Alternate Setting #0 ...
Determining device status: state = dfuIDLE, status = 0
dfuIDLE, continuing
DFU mode device DFU version 0110
Device returned transfer size 4096
Copying data from PC to DFU device
Download [=========================] 100% 552 bytes
Download done.
state(7) = dfuMANIFEST, status(0) = No error condition is present
state(2) = dfuIDLE, status(0) = No error condition is present
Done!
+ dfu-util -a 0 -e
dfu-util 0.9
Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2016 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to http://sourceforge.net/p/dfu-util/tickets/
Opening DFU capable USB device...
ID 0483:df11
Run-time device DFU version 0110
Claiming USB DFU Interface...
Setting Alternate Setting #0 ...
Determining device status: state = dfuIDLE, status = 0
dfuIDLE, continuing
DFU mode device DFU version 0110
Device returned transfer size 4096
+ sleep 5
+ dfu-util -a 0 -D build/tmp-glibc/deploy/images/ccproa1r/arm-trusted-firmware/tf-a-stm32mp133a-ccproa1r-spinand.stm32
dfu-util 0.9
Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2016 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to http://sourceforge.net/p/dfu-util/tickets/
dfu-util: Invalid DFU suffix signature
dfu-util: A valid DFU suffix will be required in a future dfu-util release!!!
Opening DFU capable USB device...
ID 0483:df11
Run-time device DFU version 0110
Claiming USB DFU Interface...
Setting Alternate Setting #0 ...
Determining device status: state = dfuIDLE, status = 0
dfuIDLE, continuing
DFU mode device DFU version 0110
Device returned transfer size 4096
Copying data from PC to DFU device
Download [=========================] 100% 84748 bytes
Download done.
dfu-util: unable to read DFU status after completion
+ dfu-util -a 0 -e
dfu-util 0.9
Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2016 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to http://sourceforge.net/p/dfu-util/tickets/
Opening DFU capable USB device...
ID 0483:df11
Run-time device DFU version 0110
Claiming USB DFU Interface...
Setting Alternate Setting #0 ...
dfu-util: Cannot set alternate interfaceI tried also download only the multivolume file and it ends abruptly with this error:
+ dfu-util -a 3 -D build/tmp-glibc/deploy/images/ccproa1r/ccproa1r-hwv-image-eng-ccproa1r_spinand_2_128_multivolume.ubi
dfu-util 0.9
Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2016 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to http://sourceforge.net/p/dfu-util/tickets/
dfu-util: Invalid DFU suffix signature
dfu-util: A valid DFU suffix will be required in a future dfu-util release!!!
Opening DFU capable USB device...
ID 0483:df11
Run-time device DFU version 0110
Claiming USB DFU Interface...
Setting Alternate Setting #3 ...
Determining device status: state = dfuIDLE, status = 0
dfuIDLE, continuing
DFU mode device DFU version 0110
Device returned transfer size 4096
Copying data from PC to DFU device
Download [= ] 4% 1806336 bytesdfu-util: Error during download get_statusIt looks like it's working, but after writing 1.7MB it crashes.
The USB download gadget is always available while the procedure is running, I can't see any problem or disconnection.
Any Idea?
Solved! Go to Solution.
2025-06-23 5:53 AM
The issue has been solved with a workaround.
Here is the debug and the solution we found.
The poor read/write performance on QSPI NAND flash was related to the assignment of pin GPIO PF8 as QSPI_IO0 line. This is a common choice for connecting a QSPI flash in new designs, but the issue is that the same GPIO line PF8 is the default wakeup IRQ line in OPTEE:
For this reason, during every QSPI communication there were a IRQ flood under OPTEE, and a resulting CPU overload (the optee overload is not directly visible under u-boot or Linux kernel).
A temporary workaround consists in not initializing the optee wakeup driver:
@@ -884,13 +880,14 @@ static TEE_Result stm32_pmic_init_it(const void *fdt, int node)
int wakeup_parent_node = 0;
int len = 0;
+ return TEE_SUCCESS;
+
Cheers
Giuseppe
2025-06-20 12:07 AM
Hi @angeloc ,
Investigation of this kind of issue deserve to have complete description of your USB implementation and configuration. (schematics, dts)
You will get a better support opening a ticket to https://ols.st.com/s/
Olivier
2025-06-20 5:19 AM - edited 2025-06-20 5:21 AM
The problem is simple, I added a bit of debug output to show that everything is correctly configured:
STM32MP> mtd list
stm32_qspi spi@58003000: stm32_qspi_probe: regs=<0x58003000> mapped=<0x70000000> mapped_size=<0x10000000>
stm32_qspi spi@58003000: regs=58003000, speed=266500000, clk=133000000
stm32_qspi spi@58003000: regs=58003000, mode=9216 rx: quad, tx: quad
spi-nand: spi_nand mt29f4g01abafdwb@0: Micron SPI NAND was found.
spi-nand: spi_nand mt29f4g01abafdwb@0: 512 MiB, block size: 256 KiB, page size: 4096, OOB size: 256
List of MTD devices:
* spi-nand0
- device: mt29f4g01abafdwb@0
- parent: spi@58003000
- driver: spi_nand
- path: /soc/bus@5c007000/spi@58003000/mt29f4g01abafdwb@0
- type: NAND flash
- block size: 0x40000 bytes
- min I/O: 0x1000 bytes
- OOB size: 256 bytes
- OOB available: 126 bytes
- 0x000000000000-0x000020000000 : "spi-nand0"
- 0x000000000000-0x000000200000 : "fsbl1"
- 0x000000200000-0x000000600000 : "fip1"
- 0x000000600000-0x000000a00000 : "fip2"
- 0x000000a00000-0x000020000000 : "UBI"
STM32MP> mtd erase spi-nand0
Erasing 0x00000000 ... 0x1fffffff (2048 eraseblock(s))
STM32MP> time mtd write spi-nand0 $loadaddr 0 0x100000
Writing 1048576 byte(s) (256 page(s)) at offset 0x00000000
time: 2 minutes, 30.543 secondsSo, the QSPI is correctly configured (both rx and tx are quad and the clock is correct), but writing a megabyte on the spi takes 2 minutes instead of nearly a second.
Cannot say the cause, still investigating.
2025-06-23 5:53 AM
The issue has been solved with a workaround.
Here is the debug and the solution we found.
The poor read/write performance on QSPI NAND flash was related to the assignment of pin GPIO PF8 as QSPI_IO0 line. This is a common choice for connecting a QSPI flash in new designs, but the issue is that the same GPIO line PF8 is the default wakeup IRQ line in OPTEE:
For this reason, during every QSPI communication there were a IRQ flood under OPTEE, and a resulting CPU overload (the optee overload is not directly visible under u-boot or Linux kernel).
A temporary workaround consists in not initializing the optee wakeup driver:
@@ -884,13 +880,14 @@ static TEE_Result stm32_pmic_init_it(const void *fdt, int node)
int wakeup_parent_node = 0;
int len = 0;
+ return TEE_SUCCESS;
+
Cheers
Giuseppe
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.