2020-11-18 5:59 PM
Hi All
When building "Eco system V2.1.0" distribution of Custom Board based on STM32MP151C chip, there is a problem that devicetree symbolic link is not created.
Symbolic link of custom board devicetree is not created in "tmp-glibc/work-shared/stm32mp1-fiscal/kernel-source/arch/arm/boot/dts" folder.
"TF-A" and "U-Boot" also do not create symbolic link of custom board device tree.
Due to the above, an error occurs because there is no "xxxxxxx.dtb" file when building with the "bitbake st-image-core" command.
Please let me know if there is a way to fix it without manually creating the symbolic link.
Thanks and regards
Machilus
Solved! Go to Solution.
2020-11-19 12:56 AM
I solved the above problem.
ENABLE_CUBEMX_DTB ?= "1"
I added the above values to the ".conf" file for custom board configuration.
2020-11-19 12:56 AM
I solved the above problem.
ENABLE_CUBEMX_DTB ?= "1"
I added the above values to the ".conf" file for custom board configuration.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.