2021-07-26 12:44 PM
Help on customizing the device tree
I installed my starter package according to instructions at https://wiki.st.com/stm32mpu/wiki/STM32MP15_Discovery_kits_-_Starter_Package
And the developer package following instructions at https://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package
Then on developing my projects, I realized that I need a different device tree than what was provided in those two packages, because the CAN bus is not defined in those installations, and that is the core of my project.
Then I read this blog
https://wiki.st.com/stm32mpu/wiki/How_to_cross-compile_with_the_Developer_Package
Somewhere, it requires to navigate to "Device Drivers - Generic Driver Options"
The problem is: if you follow those instructions, there is no option to select “Size in Megabytes,�? which left in darkness!!
Somewhere in the next page it advises to change directory to the <Linux kernel build directory> as
PC $> cd <Linux kernel build directory>
Problem is that no clear information on what this <Linux kernel build directory> is!
Again, on the next page there is this instruction
PC $> cd <Linux kernel source directory>
The following several pages keep jumping between <Linux kernel source directory> which is not clearly defined, and the <Linux kernel build directory> and then comes
PC $> cd <tag>/sources/arm-<distro>-linux-gnueabi
Where the so called <tag> and <distro> are not clearly defined
On modifying u-boot, there is the command
PC $> cd <U-Boot source directory>
and I have no idea what the <U-Boot source directory> directory is. I believe If I gent into that directory, the following instructions should be easy to fulfil, but I don’t know where that directory is. Finally there is this command with a similar problem about <TF-A source directory>
PC $> cd <TF-A source directory>
Another document I read is this
https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package
Section 3 states the prerequisistes which are in agreement with my prior process of installing of the Starter package and Developer package. However, Section 4 suggests something that I have to reinstall the developer package again, which is what I fail to understand why if I have already met the prerequisites of Section 3. If I skip Section 4, then it seems that Section 5 does not work at all.
This document relies on WORKDIR, which in my case (following instructions at https://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package) would be
$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Developer-Package
But unfortunately it does not work, which means the instructions at
https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package
are different from those at
https://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package
which bothers me.
Can I get any help on how to customize my device tree?
Solved! Go to Solution.
2021-07-27 6:34 AM
Hi @MSele.1 ,
Ok I think I got it .
https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package seems to not follow same rules than https://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package and https://wiki.st.com/stm32mpu/wiki/How_to_cross-compile_with_the_Developer_Package#Modifying_the_Linux_kernel_device_tree
So I recommand to ignore https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package and stick on the other ones.
As a summary :
For <working directory absolute path> we recommend <whatever you want>/STM32MP15-Ecosystem-v3.0.0/
So in your case <working directory absolute path> = "$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/"
Then all is relative from this folder.
<Linux kernel installation directory> is
<working directory absolute path>/Developer-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0
<Linux kernel source directory>
<working directory absolute path>/Developer-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/linux-5.10.10
<Linux kernel build directory> in case :
* Compile and install on a build directory
-> <working directory absolute path>/Developer-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/build
else same as <Linux kernel source directory>
<SDK installation directory> is <working directory absolute path>/Developer-Package/SDK
Hope it help
Olivier
2021-07-27 12:06 AM
Hi @MSele.1 ,
Thanks for your post and sorry for inconvenience using the wiki.
To get what we call "source directory" I think it can be helpful to refer to
https://wiki.st.com/stm32mpu/wiki/Example_of_directory_structure_for_Packages
For reference to <Linux kernel build directory> in
you have to know that this page consider you already build Linux a first time following :
"build directory" may depends you have decided to use in-tree or "out-tree with build folder" build mode.
For "“Size in Megabytes,�? which left in darkness!!" problem .. I will have a look
But I don't think you need to change kernel configuration just to enable CAN in device tree, right ?
Let me know if this is clearer.
Olivier
2021-07-27 5:51 AM
Thank you; the information at https://wiki.st.com/stm32mpu/wiki/Example_of_directory_structure_for_Packages provides information about some directories. However, if I followed installation instructions at https://wiki.st.com/stm32mpu/wiki/STM32MP15_Discovery_kits_-_Starter_Package
and at https://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package to the letter without deviating, what will be my <Linux kernel build directory>? Is it same as the <Linux kernel installation directory> or the <SDK installation directory>?
On another note, I just installed the starter and the developer packages only; I did not install the distribution package. Was that a mistake?
2021-07-27 6:34 AM
Hi @MSele.1 ,
Ok I think I got it .
https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package seems to not follow same rules than https://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package and https://wiki.st.com/stm32mpu/wiki/How_to_cross-compile_with_the_Developer_Package#Modifying_the_Linux_kernel_device_tree
So I recommand to ignore https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package and stick on the other ones.
As a summary :
For <working directory absolute path> we recommend <whatever you want>/STM32MP15-Ecosystem-v3.0.0/
So in your case <working directory absolute path> = "$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/"
Then all is relative from this folder.
<Linux kernel installation directory> is
<working directory absolute path>/Developer-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0
<Linux kernel source directory>
<working directory absolute path>/Developer-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/linux-5.10.10
<Linux kernel build directory> in case :
* Compile and install on a build directory
-> <working directory absolute path>/Developer-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/build
else same as <Linux kernel source directory>
<SDK installation directory> is <working directory absolute path>/Developer-Package/SDK
Hope it help
Olivier
2021-07-27 7:27 AM
Thank you; this helps a lot. I have just uninstalled all prior installations to start afresh. I will bring my feedback after the whole process. Do you think I should also install the distribution package? is it necessary?
2021-07-27 7:51 AM
Good to know it help, thanks !
For Distribution package, for you current need of just updating dts I would say no .. but it depends what you want to do afterward.
I recommend to read :
https://wiki.st.com/stm32mpu/wiki/Which_STM32MPU_Embedded_Software_Package_better_suits_your_needs
Olivier
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2021-07-27 9:03 PM
It seems my things are going much better now than before. In the past I have been using the default u-boot and TF-A that comes with the starter package. Now I start to understand that I can modify them. I just finished compiling u-boot using these commands
PC $> make stm32mp15_trusted_defconfig
PC $> make DEVICE_TREE=stm32mp157f-dk2 all
The problem, is on how to upload them into the board. The information provided at the wiki ( README_HOWTO.txt) indicates that I have to use STM32Cube-Programmer but no clear directions are provided. Any help on that step please?
The following information, which I got on the wiki is not clear to me:
PC $> STM32_Programmer_CLI -c port=usb1 \
-d tf-a_usb.stm32 0x1 -s 0x1 \
-d flashlayout.stm32 0x0 -s 0x0 \
-d fip.bin 0x3 -s 0x3
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.