2021-06-08 6:20 AM
Helllo i configurated my Device tree so i a can use my USART3 as a serdev. But when i run "cat /proc/tty/driver/stm32-usart". i can see my serial port but my RTS pin is missing. I configurated my device tree like this:
&usart3 {
pinctrl-names = "default", "sleep", "idle";
pinctrl-0 = <&usart3_pins_c>;
pinctrl-1 = <&usart3_sleep_pins_c>;
pinctrl-2 = <&usart3_idle_pins_c>;
uart-has-rtscts;
status = "ok";
ethernet {
compatible = "st,stm32_usart_net";
local-mac-address = [ A0 B0 C0 D0 E0 F0 ];
};
};
So But if i remove the ethernet part it shows the RTS port. Why is that happening?
2021-06-08 8:10 AM
I need to correct myself. It only happens when my driver is not loaded as soon as i atach the serdev it shows up. But i am not able to change The RTS pin with this command serdev_device_set_tiocm(serdev, TIOCM_RTS, 0);. My hardware flow control is disabled. Anyone had a simular problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.