2019-09-28 7:32 AM
Followed this
https://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package#Starting_up_the_SDK
and this
https://wiki.st.com/stm32mpu/nsfr_img_auth.php/5/57/U-Boot.README.HOW_TO.txt
at:
make stm32mp15_trusted_defconfig
make DEVICE_TREE=stm32mp157c-dk2 all
build goes fine but no .stm32 files in ../build-trusted
it shows:
-rw-r--r-- 1 user user 932 Sep 28 21:38 Makefile
drwxr-xr-x 4 user user 4096 Sep 28 21:35 scripts
lrwxrwxrwx 1 user user 184 Sep 28 21:38 source -> <path>/u-boot-stm32mp-2018.11-r0/build-trusted
Same for
make stm32mp15_basic_defconfig
make DEVICE_TREE=stm32mp157c-dk2 all
nor does this result in any files
make -f $PWD/../Makefile.sdk all
gives an rror:
cp: cannot stat <path>/Developer-Package/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/sources/arm-openstlinux_weston-linux-gnueabi/u-boot-stm32mp-2018.11-r0/build-basic/../build-trusted/u-boot.stm32': No such file or directory
cp: cannot stat '<path>/Developer-Package/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/sources/arm-openstlinux_weston-linux-gnueabi/u-boot-stm32mp-2018.11-r0/build-basic/../build-trusted/u-boot': No such file or directory
Ubuntu 19.04
Solved! Go to Solution.
2023-09-15 11:04 PM
Gave up on using the makefile.sdk and just use make without it
it would be nice to have a WIKI for custom board bring up as there are so many manual changes in DT and .mk files involved. Not much hope anyone who can push such forward will read this message anyhow.. :face_with_tears_of_joy:
2019-09-29 4:41 AM
To answer my own question after hours of digging:
1. the txt file instructions missed the step:
export KBUILD_OUTPUT=../build/basic
2.The doc step to move into the source filder is incorrect and should be
cd stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/sources/arm-openstlinux_weston-linux-gnueabi/u-boot-stm32mp-2018.11-r
3.The instruction guide to https://wiki.st.com/stm32mpu/wiki/How_to_cross-compile_with_the_Developer_Package#Modifying_the_U-Boot to modify the kernel , but the step
make -f $PWD/../Makefile.sdk all UBOOT_CONFIGS=stm32mp15_trusted_defconfig,trusted,u-boot.stm32
Won't work 9probably because the environment is different) so need to go back to the .txt file and follow those steps
It would be advisable if ST would try to follow the instructions once themselves to see if all is correct or not and update the documentation.There are many links connected abouyt the STM32MP1 but they seem not work well together.
2023-09-15 11:04 PM
Gave up on using the makefile.sdk and just use make without it
it would be nice to have a WIKI for custom board bring up as there are so many manual changes in DT and .mk files involved. Not much hope anyone who can push such forward will read this message anyhow.. :face_with_tears_of_joy:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.