2020-01-16 7:23 PM
I want to configure the TFTP launch, but I can't generate the core-image-least-initramfs system
2020-01-22 12:40 AM
Hi @昌�?� �?�
Thanks to raise this point.
This is actually an error in the wiki since the default Yocto settings provides initramfs for x86 HOST and not for ARM.
The wiki article will be modified as follow :
To fully boot on a network (kernel and rootfs), the rootfs to use can be defined :
initramfs is only one solution among several for the rootfs.
If it is really the solution you are targeting you can follow any generic tutorial on the web related to uInitrd creation. ( with or without Yocto)
Hope it help,
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.