STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to enable a third party 3.5" Display connected to LTDC port on STM32MP157C-EV1 board?

I need to test a 3.5" display connected to the LTDC port. How do I disable the 5.5" display that came with the STM32MP157C-EV1 board and use the 3.5" display? I see the ltdc_pins_a: ltdc-a-0{...} entry in the Linux source code device tree: ../linux-4...

Resolved! problems with installing fftw package

Hi! Have some problems with installing fftw package. I tried to install it to st-image-weston and st-example-image-xfce, but received same error when bitbake run do_rootfs. Can anybody explain this problem?Build Configuration:BB_VERSION          = "1...

VKare.1 by Associate II
  • 2175 Views
  • 1 replies
  • 0 kudos

Resolved! Hello. We are trying to reset MCU from within MCU by asserting SYSRESETREQ it in Cortex M4 AIRCR register (by calling NVIC_SystemReset). After that the MCU halts and FW is not running.

If we emulate the MCU watchdog reset on STM32MP1 it works fine. MCU is got restarted and runs after that. SYSRESETREQ assertion (by calling NVIC_SystemReset) works fine with dedicated M4 processor.We wander what can be a problem on STM32MP1 ?

dimax by Senior
  • 6445 Views
  • 10 replies
  • 0 kudos

Resolved! gcnano is not install in rootfs

I built the rootfs according to the instructions at https://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package, but the userspace program of gcnano is not installed in the rootfs, the / vendor directory is empty. I need to manually install gcnan...

Jzhua by Associate III
  • 2019 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.