2019-09-30 9:02 PM
Can't a7-core write firmware with a generic compiler like IAR without Linux?
Like working with tools like ADS Compiler , like s3c6440 .....
2019-09-30 10:33 PM
You can compile with GNU/GCC running under Windows.
2019-09-30 10:42 PM
You need to check if the compiler supports the specific core (Cortex A7), and the toolchain comes with the required environment (Linux header files, device-specific drivers, and libs).
Microcontroller specific ones like IAR and Keil usually do not.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.