STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Authentication of the M4 Firmware

Hi There,before I go into detail regarding my question I´d like to give some background infos. I have an application in mind that seems like a perfect fit for the STM32MP1 as it would enable me to merge a device which is currently split onto two sepa...

Multiples Content Coherence Issue between STM32CubeMP1 and STM32MP15x Reference Manual

Hello,We are currently building a product using a STM32MP157 processor and are facing multiples discrepancies between the Reference Manual and the STM32MP1 Cube Package.STM32CubeMP1 register memory map :https://github.com/STMicroelectronics/STM32Cube...

Android support

Hello,Could you explain the reason why Android is not supported on the STM32MP157C-DK2?I can't find any instructions how to install an Android image on the target? The following example references the coprocessor example for A7 and M4 cores, but miss...

Resolved! STM32MP153a failed to boot from eMMC.

Hi there, I am working with a customized STM32MP153A board and trying to boot from eMMC.​I had prepared my eMMC following the steps that I found in <u-boot-stm32mp-2018.11-r0 source code directory>/board/st/stm32mp1/README file:​8. Prepare eMMC======...

BryanWang by Associate II
  • 6588 Views
  • 8 replies
  • 0 kudos

Resolved! STPMIC1 - PONKEYn POWER_ON POWER_DOWN trigger

For STPMIC1, when it is powered on by asserting the PONKEYn signal low, what would happen if the PONKEYn remains asserted low even after the initial POWER_ON trigger? Would it subsequently trigger a POWER_DOWN if PONKEYn long press turn off is activa...

SYEH by Associate II
  • 2631 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.